2008-06-22 14:25:33     directfb pkgconfig problem

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-22 14:25:33     directfb pkgconfig problem

Michael Weber (UNITED STATES)

Message: 57682   

 

I'm not sure if I'm doing something wrong or if there's a problem with the build process, but it seems that the pkgconfig files for directfb are not generated correctly in the staging area.  They simply reference /usr in the prefix, not the full path to the staging area.  I tried to look at the difference between the configure logs between directfb and libpng (which generates the right pc file), but I could see anything.  Does anyone have any ideas?

QuoteReplyEditDelete

 

 

2008-06-22 15:00:03     Re: directfb pkgconfig problem

Michael Weber (UNITED STATES)

Message: 57683   

 

I figured it out -- the library I added that had a dependency on directfb was added as dir_5 in the root lib Makefile, but directfb is also dir_5, so the root makefile didn't have a chance to fix the pc files in the staging area.  All I had to do was change the added library to dir_6 and it picked up the fixed pc file.

Attachments

    Outcomes