2008-06-19 11:16:30     BF533-Stamp - Ethernet Crash with Xenomai

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-19 11:16:30     BF533-Stamp - Ethernet Crash with Xenomai

wolfgang hiess (AUSTRIA)

Message: 57589   

 

Hi!

 

Dist: 2008R1-RC8 with XENOMAI 2.4.0

 

After assigning an IP-Address, the board displays some error messages and a few seconds later it hangs.

 

Can anybody help me with this problem?

 

Thanks and regards,

Wolfgang

 

 

 

Output:

 

ifconfig eth0 10.9.24.65

eth0: link down

root:/> eth0: link up, 10Mbps, half-duplex, lpa 0x0021

 

root:/> ping 10.9.24.67

PING 10.9.24.67 (10.9.24.67): 56 data bWtesARNING: at kernel/softirq.c:138 local_bh_enable()

Hardware Trace:

   0 Target : <0x000047fc> { _dump_stack + 0x0 }

     Source : <0x00012ec0> { _local_bh_enable + 0x8c }

   1 Target : <0x00012ec0> { _local_bh_enable + 0x8c }

     Source : <0x0000e516> { _printk + 0x5a }

   2 Target : <0x0000e50c> { _printk + 0x50 }

     Source : <0x0000e390> { _vprintk + 0x1d4 }

   3 Target : <0x0000e384> { _vprintk + 0x1c8 }

     Source : <0x0002c9f6> { ___ipipe_restore_root + 0x46 }

   4 Target : <0x0002c9b0> { ___ipipe_restore_root + 0x0 }

     Source : <0x0000e380> { _vprintk + 0x1c4 }

   5 Target : <0x0000e37e> { _vprintk + 0x1c2 }

     Source : <0x0000e1b6> { _wake_up_klogd + 0x36 }

   6 Target : <0x0000e1b2> { _wake_up_klogd + 0x32 }

     Source : <0x0002c9f6> { ___ipipe_restore_root + 0x46 }

   7 Target : <0x0002c9b0> { ___ipipe_restore_root + 0x0 }

     Source : <0x0000b2fc> { ___wake_up + 0x4c }

   8 Target : <0x0000b2f2> { ___wake_up + 0x42 }

     Source : <0x0000a20a> { ___wake_up_common + 0x52 }

   9 Target : <0x0000a1fc> { ___wake_up_common + 0x44 }

     Source : <0x0000a1f2> { ___wake_up_common + 0x3a }

  10 Target : <0x0000a1ec> { ___wake_up_common + 0x34 }

     Source : <0x0001ec58> { _autoremove_wake_function + 0x2c }

  11 Target : <0x0001ec3e> { _autoremove_wake_function + 0x12 }

     Source : <0x0000b014> { _try_to_wake_up + 0x40 }

  12 Target : <0x0000b00c> { _try_to_wake_up + 0x38 }

     Source : <0x0002c9f6> { ___ipipe_restore_root + 0x46 }

  13 Target : <0x0002c9b0> { ___ipipe_restore_root + 0x0 }

     Source : <0x0000b008> { _try_to_wake_up + 0x34 }

  14 Target : <0x0000b002> { _try_to_wake_up + 0x2e }

     Source : <0x0000b0a8> { _try_to_wake_up + 0xd4 }

  15 Target : <0x0000b0a6> { _try_to_wake_up + 0xd2 }

     Source : <0x0000b084> { _try_to_wake_up + 0xb0 }

Stack from 0047be70:

        00497fc8 00012ec4 00497fc8 00000000 000e2060 00153e88 0000008a 00128c74

        000e1fb4 0311d800 4318090a 0311d800 4118090a 0010f82c 0311ff00 03592820

        00486a00 00015dcc 0001be90 0017be00 0311d800 4118090a 00000000 0311d930

        00000000 000e681c 03592820 00486a00 0017be00 00000003 00000000 00000100

        0017d5f4 0047bf30 00015904 004981c0 00015a08 004981c0 0047bf28 000e66e8

        03592820 0047a000 00499da0 00000017 0017cd34 00000000 0047bf28 0047bf28

 

Call Trace:

[<00012acc>] ___do_softirq+0x60/0xc4

[<000089b8>] _do_irqd+0xc0/0x138

[<00008a00>] _do_irqd+0x108/0x138

[<0001ea08>] _kthread+0x50/0x64

[<000088f8>] _do_irqd+0x0/0x138

[<00001686>] _kernel_thread_helper+0x6/0xc

 

 

64 bytes from 10.9.24.67: icmp_seq=0 ttl=64 time=29.2 ms

64 bytes from 10.9.24.67: icmp_seq=1 ttl=64 time=0.6 ms

64 bytes from 10.9.24.67: icmp_seq=2 ttl=64 time=0.6 ms

64 bytes from 10.9.24.67: icmp_seq=3 ttl=64 time=0.5 ms

 

*board hangs*

Attachments

    Outcomes