2008-06-09 02:22:37     Could not find MAX 1233 driver in uClinux Dist

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-09 02:22:37     Could not find MAX 1233 driver in uClinux Dist

V Hemanth Kumar (INDIA)

Message: 56850   

 

Hi,

 

We are using BF527 EZKit, trying to test the touch screen, (MAX 1233 on BF527 EZKit).

 

I could not find the driver for the MAX 1233 in the "uclinux distribution's->Device Drivers->input device support->Touchscreens".

 

So is this peripheral (driver) not supported or developed?

 

Regards,

 

Hemanth Kumar.V

QuoteReplyEditDelete

 

 

2008-06-09 02:52:51     Re: Could not find MAX 1233 driver in uClinux Dist

Mike Frysinger (UNITED STATES)

Message: 56851   

 

please review the board documentation as it covers this:

http://docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf527-ezkit#touchscreen_keypad

QuoteReplyEditDelete

 

 

2008-06-09 04:41:44     Re: Could not find MAX 1233 driver in uClinux Dist

V Hemanth Kumar (INDIA)

Message: 56860   

 

Thanks for the info Mike.

QuoteReplyEditDelete

 

 

2008-06-09 08:45:02     Re: Could not find MAX 1233 driver in uClinux Dist

Konstantin Hartwich (GERMANY)

Message: 56866   

 

i have posted a mod of the old ad7877 touchscreen driver some weeks ago..none seemd to be interested.

 

i am using it. its kind of stable for now..search for it here in the forum. if zou encounter problems post it..

QuoteReplyEditDelete

 

 

2008-06-11 01:09:42     Re: Could not find MAX 1233 driver in uClinux Dist

V Hemanth Kumar (INDIA)

Message: 56959   

 

I have downloaded your max1233 driver code. I will try to use it...Thanks

QuoteReplyEditDelete

 

 

2008-06-11 11:02:21     Re: Could not find MAX 1233 driver in uClinux Dist

Robin Getz (UNITED STATES)

Message: 57002   

 

Konstantin:

 

The best thing to do with that driver - would be to send it upstream - to the kernel mailing list, and see what feedback you get on it.

 

-Robin

Attachments

    Outcomes