2008-06-10 12:46:48     On BF537 EZ-KIT, AD1854 and uClinux

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-10 12:46:48     On BF537 EZ-KIT, AD1854 and uClinux

Nicola Bonelli (ITALY)

Message: 56941   

 

In some previous posts I have read that it's possible to use the built in AD1854 DAC on BF537 EZ-KIT

running uClinux.

 

In particular it should be possible to use the driver for the AD1836. Instead I'm experiencing some problems.

When I try to modprobe the module I get the following error:

 

AD1836 Card is not attached

 

Do I miss something ? I'm running the kernel 2.6.22.18-ADI-2008R1-svn...

 

Any help is appreciated...

Thanks in advance,

 

 

Nicola

QuoteReplyEditDelete

 

 

2008-06-10 13:09:30     Re: On BF537 EZ-KIT, AD1854 and uClinux

Mike Frysinger (UNITED STATES)

Message: 56942   

 

please review: http://docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf537-ezkit

Attachments

    Outcomes