2008-06-10 04:33:18     error compiling cpu frequency scalling

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-10 04:33:18     error compiling cpu frequency scalling

Bastien Briec (FRANCE)

Message: 56911   

 

Hello, while trying to compile cpu frequency scalling I get the following error :

 

  --support-old-code   supporter les veilles versions de code

  --support-old-code   supporter les veilles versions de code

/opt/uClinux/bfin-uclinux/bin/bfin-uclinux-ld.real: utilisation ill�gale de la section � .initcall0.init �

make[1]: *** [.tmp_vmlinux1] Erreur 1

make[1]: quittant le répertoire « /home/bgt/uClinux-dist/linux-2.6.x »

make: *** [linux] Erreur 1

bgt@debian:~/uClinux-dist$

 

I use the 2007 release, may this error be resolved using 2008 release or here is another way?

TranslateQuoteReplyEditDelete

 

 

2008-06-10 10:47:33     Re: error compiling cpu frequency scalling

Mike Frysinger (UNITED STATES)

Message: 56933   

 

the cpu scaling code really wasnt usable in 2007R1.  it has since been rewritten and is stable in svn trunk.

 

 

2008-06-10 07:59:19     Re: is it possible to run Threads on core B

Robin Getz (UNITED STATES)

Message: 56924   

 

Stephen:

 

Not possible. Do split threads across cores would require a cache coherant system.

 

The best you can do is run Application A on Core A, and Application B on core B - but they can not share memory.

Attachments

    Outcomes