2008-06-09 02:16:12     some problems about UART and PPI on bf537 ezkit

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-09 02:16:12     some problems about UART and PPI on bf537 ezkit

edward jiang (CHINA)

Message: 56849   

 

Hi all:

 

         Form the bf537 ezkit lite schematic, I noticed that UART0 is composed of 4 pins : PF0,PF1,PG6,PG7; but PG6 and PG7 is also PPI_DATA_6 and PPI_DATA_7 .

 

          My question is:  if i use uclinux on 537 , then  UART0 will be the terminal for the OS , also PG6 and PG7 is used as the terminal pins . Does it means that i can't use PPI at the same time??  How to fix this ?  thanks 

QuoteReplyEditDelete

 

 

2008-06-09 02:54:22     Re: some problems about UART and PPI on bf537 ezkit

Mike Frysinger (UNITED STATES)

Message: 56852   

 

the schematics show how two of the pins are multiplexed and not hooked up by default

Attachments

    Outcomes