2008-06-04 07:35:34     Extract kernel configuration from a device

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-04 07:35:34     Extract kernel configuration from a device

Vincent Puig (SPAIN)

Message: 56676   

 

Hi all,

 

is it posible to extract the kernel configuration from a device?.

 

I have 2 Bluetechnix modul, CM-BF537E. I want to know the kernel configuration of one of them, so I could have a look to the options it has enabled, and I would enable the same options to the other.

 

If I had the file .config it would be easier, but I haven't. It wasn't configured and compiled in the same computer I am.  Is there any way to do that?.

 

I don't want to copy and paste, I want to see the configuration file.

QuoteReplyEditDelete

 

 

2008-06-04 16:32:35     Re: Extract kernel configuration from a device

Mike Frysinger (UNITED STATES)

Message: 56695   

 

only if the kernel was configured to include its config in it.  if /proc/config.gz exists, you can use that.  if it doesnt exist, there's no way to know what config was used to build the kernel.

QuoteReplyEditDelete

 

 

2008-06-05 17:46:53     Re: Extract kernel configuration from a device

Vincent Puig (SPAIN)

Message: 56765   

 

Yes, that was what I thought.

 

Thanks anyway Mike.

Attachments

    Outcomes