2008-06-03 06:28:45     nfs as rootfs

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-06-03 06:28:45     nfs as rootfs

Yi Li (CHINA)

Message: 56617   

 

Question from customer:

 

In doc: http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:nfs

 

It says:

 

"If you wish to use NFS as your root filesystem, you will also need these settings:

 

Networking  --->

  Networking options  --->

    [*] TCP/IP networking

    [*]   IP: kernel level autoconfiguration

File systems  --->

  Network File Systems  --->

    [*] Root file system on NFS

    [*] Support for rpcbind versions 3 & 4"

 

But cannot find the option "[*] Root file system on NFS" in 2008R1 release. Is the document obsolete?

 

 

QuoteReplyEditDelete

 

 

2008-06-03 10:23:23     Re: nfs as rootfs

Mike Frysinger (UNITED STATES)

Message: 56628   

 

the documentation is not out of date ... the option will only show up if you've properly selected other options

QuoteReplyEditDelete

 

 

2008-06-03 23:40:21     Re: nfs as rootfs

Yi Li (CHINA)

Message: 56656   

 

Ok now, CONFIG_NFS_FS need to be buillt-in, instead of building as a module. Thanks.

Attachments

    Outcomes