2008-05-30 13:42:35     vmstat doesn't work

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-05-30 13:42:35     vmstat doesn't work

Joao Paulo Bodanese (BRAZIL)

Message: 56480   

 

HI,

 

root:~> vmstat 1 100

   procs                      memory    swap          io     system         cpu

o   b  w   swpd   free   buff  cache  si  so    bi

n

nter access (probably)

 

CURRENT PROCESS:

 

COMM=vmstat PID=159

TEXT = 0x00868000-0x0086bbc8  DATA = 0x01030bc8-0x0103269c

BSS = 0x0103269c-0x01060000   USER-STACK = 0x0107feb0

 

return address: 0x02a9da0e; contents of [PC-16...PC+8]:

3008 2006 3209 9948 0c00 181a 6409 6018

5401 0c00 17f8 3211 e141 fefe e101 feff X

9010 5008 e141 8080 e101 8080 5408 0c00

 

RETE:  00000000  RETN: 0102e000  RETX: 02a9da0e  RETS: 02a9c968

IPEND: 0030  SYSCFG: 0036

SEQSTAT: 00060027    SP: 0102df24

R0: 00000000    R1: fefefeff    R2: 00000000    R3: 00000003

R4: 0107fc58    R5: 0086b630    R6: 010398b8    R7: 00000000

P0: 0107fc20    P1: 00000005    P2: 00000000    P3: 010398b8

P4: 01031024    P5: 01031028    FP: 0107fbcc

A0.w: 00000000    A0.x: 00000000    A1.w: 00000000    A1.x: 00000000

LB0: 02a9d503  LT0: 02a9d502  LC0: 00000000

LB1: 0086a0bb  LT1: 0086a0ac  LC1: 00000000

B0: 00000007  L0: 00000000  M0: 00000000  I0: 02ab250c

B1: 00000000  L1: 00000000  M1: 00000000  I1: 00000000

B2: 00000000  L2: 00000000  M2: 00000000  I2: 00000000

B3: 00000000  L3: 00000000  M3: 00000000  I3: 0107fd44

 

USP: 0107fbcc   ASTAT: 02003025

DCPLB_FAULT_ADDR=00000000

ICPLB_FAULT_ADDR=02a9da0e

 

 

Hardware Trace:

0 Target : <0x00004580> { _trap_c + 0x0 }

   Source : <0xffa00b50> { _exception_to_level5 + 0xb4 }

1 Target : <0xffa00a9c> { _exception_to_level5 + 0x0 }

   Source : <0xffa00a9a> { _ex_trap_c + 0x4e }

2 Target : <0xffa00a4c> { _ex_trap_c + 0x0 }

   Source : <0xffa00bf0> { _trap + 0x28 }

3 Target : <0xffa00bc8> { _trap + 0x0 }

   Source : <0x02a9da0a> [ /lib/libuClibc-0.9.29.so + 0x1da0a ]

4 Target : <0x02a9d9fc> [ /lib/libuClibc-0.9.29.so + 0x1d9fc ]

   Source : <0x02a9d9f0> [ /lib/libuClibc-0.9.29.so + 0x1d9f0 ]

5 Target : <0x02a9d9e8> [ /lib/libuClibc-0.9.29.so + 0x1d9e8 ]

   Source : <0x02a9c964> [ /lib/libuClibc-0.9.29.so + 0x1c964 ]

6 Target : <0x02a9c958> [ /lib/libuClibc-0.9.29.so + 0x1c958 ]

   Source : <0x02a9d514> [ /lib/libuClibc-0.9.29.so + 0x1d514 ]

7 Target : <0x02a9d4dc> [ /lib/libuClibc-0.9.29.so + 0x1d4dc ]

   Source : <0x02a9a896> [ /lib/libuClibc-0.9.29.so + 0x1a896 ]

8 Target : <0x02a9a888> [ /lib/libuClibc-0.9.29.so + 0x1a888 ]

   Source : <0x02a9c954> [ /lib/libuClibc-0.9.29.so + 0x1c954 ]

9 Target : <0x02a9c930> [ /lib/libuClibc-0.9.29.so + 0x1c930 ]

   Source : <0x02a9c8f4> [ /lib/libuClibc-0.9.29.so + 0x1c8f4 ]

10 Target : <0x02a9c8e8> [ /lib/libuClibc-0.9.29.so + 0x1c8e8 ]

   Source : <0x00868c5c> [ /bin/vmstat + 0xc5c ]

11 Target : <0x00868c54> [ /bin/vmstat + 0xc54 ]

   Source : <0x00869254> [ /bin/vmstat + 0x1254 ]

12 Target : <0x00869246> [ /bin/vmstat + 0x1246 ]

   Source : <0x02a9de66> [ /lib/libuClibc-0.9.29.so + 0x1de66 ]

13 Target : <0x02a9de5e> [ /lib/libuClibc-0.9.29.so + 0x1de5e ]

   Source : <0x02a9ddfc> [ /lib/libuClibc-0.9.29.so + 0x1ddfc ]

14 Target : <0x02a9ddee> [ /lib/libuClibc-0.9.29.so + 0x1ddee ]

   Source : <0x02a9de04> [ /lib/libuClibc-0.9.29.so + 0x1de04 ]

15 Target : <0x02a9ddee> [ /lib/libuClibc-0.9.29.so + 0x1ddee ]

   Source : <0x02a9de04> [ /lib/libuClibc-0.9.29.so + 0x1de04 ]

Stack from 0102df04:

        00034588 ffa00b54 0013a710 0013a710 0013a710 00000fff 0107fe0c 02a8c436

        02a9da0e 00000030 00060027 00000000 0102e000 02a9da0e 02a9da0e 02a9c968

        00000000 02003025 0086a0bb 02a9d503 0086a0ac 02a9d502 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000007

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        0107fd44 00000000 00000000 02ab250c 0107fbcc 0107fbcc 01031028 01031024

Call Trace:

 

SIGSEGV

root:~>          

 

 

 

any ideia?

 

 

 

Thanks,

 

João Paulo

QuoteReplyEditDelete

 

 

2008-05-30 18:57:46     Re: vmstat doesn't work

Mike Frysinger (UNITED STATES)

Message: 56487   

 

whatever the bug is, it appears to be fixed in newer procps.  we have 2.0.7 in our dist now, and 3.2.7 seems to work fine.

 

root:/> vmstat -V

procps version 3.2.7

root:/> vmstat

procs -----------memory---------- ---swap-- -----io---- -system-- ----cpu----

r  b   swpd   free   buff  cache   si   so    bi    bo   in   cs us sy id wa

0  0      0  46188      0   8260    0    0     0     0  251   14  0  0 100  0

Attachments

    Outcomes