2008-05-16 09:30:01     Problem with msntp client

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-05-16 09:30:01     Problem with msntp client

Pavel Frolov (BELARUS)

Message: 55927   

 

It was a problem with msntp client (from uClinux-dist-2008R1-RC8)  on BF533 EZkit-based board, while msntp server work ok. Time server, after receiving packets from BF5xx, couldn't recognize request and dosn't send answer.

 

This problem can be fixed by downloading other (newer) version of msntp or by applying patch from attachment.

 

msntp.patch.gz

QuoteReplyEditDelete

 

 

2008-05-16 09:55:25     Re: Problem with msntp client

Robin Getz (UNITED STATES)

Message: 55931   

 

Pavel:

 

Thanks for the note.

 

We have Version 1.6 in the dist. When I checked debian - that is the same version they ship (http://packages.qa.debian.org/m/msntp.html ) although, they do add a few local debian patches (plus I could not find the actual homepage of the project).

 

Do you have any pointers?

 

 

 

Thanks

 

-Robin

QuoteReplyEditDelete

 

 

2008-05-19 02:46:25     Re: Problem with msntp client

Pavel Frolov (BELARUS)

Message: 56001    As I remember, I've downloaded it from https://launchpad.net/ubuntu/+source/msntp/1.6.dfsg-2. According to header.h this is version 1.6a. Pavel. Promwad Innovation Company.

QuoteReplyEditDelete

 

 

2008-05-28 15:34:38     Re: Problem with msntp client

Mike Frysinger (UNITED STATES)

Message: 56369   

 

thanks, ive applied this patch to svn

Attachments

Outcomes