2008-05-09 16:28:28     How to create a flashable uimage for EZKIT533

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-05-09 16:28:28     How to create a flashable uimage for EZKIT533

Li Kun (CHINA)

Message: 55695   

 

Currently,I have problem with building a uimage file less than 2MB,in order to fit the size of the flash on BF533 EZKIT board.

 

I tried to trim a lot of options while compling it,but the uimage was still created at about 3~4 MB in the end.I can load uimage to the BF533 EZKITby serial port,and it runs well. But I can't cp it to the flash,simply because 2MB flash is not enough for the uimage file. Then I'll have to upload the uimage file every time I turn on the board,in order to make the uClinux running.

 

I need some help for porting uclinux to BF533 EZKIT board,where I can flash the uimage file to it.For example,how to configurate the options during the  "make menuconfig" process,or any other tips.

 

Thanks.

QuoteReplyEditDelete

 

 

2008-05-09 16:37:45     Re: How to create a flashable uimage for EZKIT533

Mike Frysinger (UNITED STATES)

Message: 55696   

 

please review the faq (My uImage is too large to burn in my flash):

http://docs.blackfin.uclinux.org/doku.php?id=faq

Attachments

    Outcomes