2008-05-02 08:55:18     send file via uart?

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-05-02 08:55:18     send file via uart?

Bastien Briec (FRANCE)

Message: 55367   

 

Hello, is it possible to send a file via uart from uClinux and get it on the host using something like sx and rx (there is not sx in busibox)? If it's possible can you tell me how?

 

regards, bastien.

TranslateQuoteReplyEditDelete

 

 

2008-05-02 18:24:34     Re: send file via uart?

Mike Frysinger (UNITED STATES)

Message: 55381   

 

just use the srz and lrz commands to transmit files using zmodem

 

i dont know what these "sx" and "rx" commands are ...

QuoteReplyEditDelete

 

 

2008-05-05 04:11:39     Re: send file via uart?

Bastien Briec (FRANCE)

Message: 55479   

 

sx and rx are unix commands to send and receive using xmodem. I look in the xconfig but I can't find srz and lrz, I use 2007r1 uClinux, are lrz and srz only present in lastest version?

TranslateQuoteReplyEditDelete

 

 

2008-05-05 04:24:57     Re: send file via uart?

Mike Frysinger (UNITED STATES)

Message: 55482   

 

no, srz and lrz have always been there.  they are the zmodem utilities.

QuoteReplyEditDelete

 

 

2008-05-05 05:31:05     Re: send file via uart?

Bastien Briec (FRANCE)

Message: 55489   

 

ok I've found thanks

TranslateQuoteReplyEditDelete

 

 

2008-05-05 08:58:51     Re: send file via uart?

Mike Frysinger (UNITED STATES)

Message: 55502   

 

as i said, they are the zmodem utilities ... so you have to enable the zmodem utilties in your vendor/user configuration

Attachments

    Outcomes