2008-04-28 10:34:39     tftp help!

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-28 10:34:39     tftp help!

zhi shaolong (CHINA)

Message: 55139   

 

i have installed tftp-server,since the IP of host is 10.12.12.1

 

and IP of colinux is 10.12.12.2

 

the host can put and get files from/to the colinux.

 

dose it demenstrate my tftp-server is ok?

 

but ,when my u-boot start,

 

i enterer bfin>tftp 0x1000000 /tftpboot/linux

 

error occurs:

 

u-boot 1.1.6 (ADI-2008R1) (Apr 14 2008 - 09:08:38)

 

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3)

Board: ADI BF533 Stamp board

       Support: http://blackfin.uclinux.org/

       Clock: VCO: 398 MHz, Core: 398 MHz, System: 79 MHz

       RAM:   128 MB

       Flash:  4 MB

       In:    serial

       Out:   serial

       Err:   serial

       Net:   SMC91111 at 0x20300300

       MAC:   00:E0:22:FE:04:50

       I2C:   ready

       Hit any key to stop autoboot:  0

       bfin> tftp 0x1000000 linux

       SMC91111: PHY auto-negotiate timed out

       TFTP from server 10.12.12.2; our IP address is 10.12.12.15

       Filename 'linux'.

       Load address: 0x1000000

       Loading: T T T T T T T T T T

       Retry count exceeded; starting again

       TFTP from server 192.168.0.2; our IP address is 192.168.0.15

       Filename 'linux'.

       Load address: 0x1000000

       Loading: *

 

could you help me ?

 

thanks a lot!

QuoteReplyEditDelete

 

 

2008-04-28 11:11:30     Re: tftp help!

Mike Frysinger (UNITED STATES)

Message: 55149    check your cables ... this error should not be there:

       SMC91111: PHY auto-negotiate timed out

QuoteReplyEditDelete

 

 

2008-04-29 23:46:32     Re: tftp help!

Pafone Lee (CHINA)

Message: 55263   

 

disable the firewall and try again.

 

and then ... it work

Attachments

    Outcomes