2008-04-26 01:43:15     how to use skyeye for bf561-ezkit?

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-26 01:43:15     how to use skyeye for bf561-ezkit?

chong yuan (CHINA)

Message: 54974   

 

first,i downloaded "skyeye-1.2-RC8-3.tar.bz2 "and exacted it in "/" directory

 

second, do "make" in "/skyeye-v1"

 

third,create a config file named <code>skyeye.conf</code> with one line in it:  "arch: blackfin" in  "/skyeye-v1"directory

 

fourth,"make AnalogDevices/BF561-EZKIT_default" in "uclinux-dist"directory and left linux file in "images"directory

 

finally, copy "/uclinux-dist/images/linux" to "/skyeye-v1" and run "skyeye -e linux" in "/skyeye-v1" ,however, following error showed:

 

[root@david skyeye-v1]# skyeye -e linux

arch: blackfin

begin init emulator()

exec file "linux"'s format is elf32-little.

load section .text: addr = 0x00001000  size = 0x000ea750.

load section .rodata: addr = 0x000ec000  size = 0x00034958.

load section __ksymtab: addr = 0x00120958  size = 0x00003638.

load section __ksymtab_gpl: addr = 0x00123f90  size = 0x00000e60.

load section __ksymtab_strings: addr = 0x00124df0  size = 0x0000a3e0.

load section __param: addr = 0x0012f1d0  size = 0x00000140.

load section .data: addr = 0x00130000  size = 0x00010000.

load section .init.text: addr = 0x00140000  size = 0x000156e0.

load section .init.data: addr = 0x001556e0  size = 0x00000cac.

load section .init.setup: addr = 0x0015638c  size = 0x00000250.

load section .initcall.init: addr = 0x001565dc  size = 0x0000018c.

load section .con_initcall.init: addr = 0x00156768  size = 0x00000004.

load section .init.ramfs: addr = 0x0015676c  size = 0x00293a12.

load section .text_l1: lma = 0x003ea17e (vma = 0xffa00000)  size = 0x00001e68.

load section .data_l1: lma = 0x003ebfe6 (vma = 0xff800000)  size = 0x000000c0.

not load section .bss: addr = 0x003ed000  size = 0x0000f570 .

not load section .comment: addr = 0x00000000  size = 0x00002990 .

start addr is set to 0x00140000 by exec file.

ssram_write_long addr 0xffb00ffc

ssram_write_long addr 0xffb00ff8

ssram_write_long addr 0xffb00ff4

ssram_write_long addr 0xffb00ff0

ssram_write_long addr 0xffb00fec

ssram_write_long addr 0xffb00fdc

ssram_write_long addr 0xffb00fd8

ssram_write_long addr 0xffb00fd4

ssram_write_long addr 0xffb00fd0

ssram_write_long addr 0xffb00fcc

ssram_read_long addr 0xffb00fcc

ssram_read_long addr 0xffb00fd0

ssram_read_long addr 0xffb00fd4

ssram_read_long addr 0xffb00fd8

ssram_read_long addr 0xffb00fdc

ssram_write_long addr 0xffb00fdc

ssram_write_long addr 0xffb00fd8

ssram_write_long addr 0xffb00fd4

ssram_write_long addr 0xffb00fd0

ssram_write_long addr 0xffb00fcc

ssram_write_long addr 0xffb00fc8

 

bf533_io_write_word io error!!!addr=0xffc01f28,pc=0x6c58

Illegal instruction

 

pls help me!

 

thank you very much!

TranslateQuoteReplyEditDelete

 

 

2008-04-26 01:52:08     Re: how to use skyeye for bf561-ezkit?

Mike Frysinger (UNITED STATES)

Message: 54975    skyeye doesnt currently support the BF561

QuoteReplyEditDelete

 

 

2008-04-26 05:19:13     Re: how to use skyeye for bf561-ezkit?

chong yuan (CHINA)

Message: 55017   

 

Thank you!

 

what about bf533?

 

if bf533 is supported,what shoud i do to use skyeye for bf533?

TranslateQuoteReplyEditDelete

 

 

2008-04-26 05:28:22     Re: how to use skyeye for bf561-ezkit?

Mike Frysinger (UNITED STATES)

Message: 55018    unfortunately, only like the 2005R3 or 2005R4 release will work

QuoteReplyEditDelete

 

 

2008-04-26 06:39:21     回复: Re: how to use skyeye for bf561-ezkit?

chong yuan (CHINA)

Message: 55021    thank you very very much!

Attachments

    Outcomes