2008-04-24 06:27:36     console through tcpip failes when disable uart console

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-24 06:27:36     console through tcpip failes when disable uart console

Servaes Joordens (NETHERLANDS)

Message: 54847   

 

In inittab I disabled the line:

 

ttyBF0::respawn:/bin/getty -L ttyBF0 115200 vt100

 

That worked well for disabling the uart-consolse, but It also disables telnet through ethernet.

 

Does anyone known how to disable the console over uart, while leavin the telnet through ethernet intact?

QuoteReplyEditDelete

 

 

2008-04-24 07:06:30     Re: console through tcpip failes when disable uart console

Michael Hennerich (GERMANY)

Message: 54852    Don't do that.

 

Simply change your kernel command line:

from console=ttyBF0,5600 to console=

 

http://docs.blackfin.uclinux.org/doku.php?id=silent_booting&s[]=console

 

-Michael

QuoteReplyEditDelete

 

 

2008-04-24 15:56:11     Re: console through tcpip failes when disable uart console

Mike Frysinger (UNITED STATES)

Message: 54894    removing that line has no affect on telnet or ethernet whatsoever

 

most likely what is happening is that you removed *all* lines from your inittab and so the init process exited because you didnt give it anything to run and then the kernel promptly paniced

QuoteReplyEditDelete

 

 

2008-04-25 03:34:57     Re: console through tcpip failes when disable uart console

Servaes Joordens (NETHERLANDS)

Message: 54925   

 

Mike,

 

I think you are right.

 

I enabled the line:

 

sh:console:respawn:-/bin/sh

 

and it worked again.

Attachments

    Outcomes