2008-04-17 04:44:43     change file wcfxs.c (si3210 driver)

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-17 04:44:43     change file wcfxs.c (si3210 driver)

hand york (JAPAN)

Message: 54397   

 

Hi, all

 

The Si3210 is the ProSLIC used for the FXS devices, and the driver is file wcfxs.c in zaptel.

 

I want to change the Si3210(wcfxs.c) driver, don't use "struct zt_span" and "struct zt_chan", it means that I can access the Si3210 (read/write) without zaptel.

 

Is there anyone do it beforen?

 

Is there any suggestions?

 

Thank you.

TranslateQuoteReplyEditDelete

 

 

2008-04-17 22:05:37     回复: change file wcfxs.c (si3210 driver)

hand york (JAPAN)

Message: 54441    Is there no suggestions?

TranslateQuoteReplyEditDelete

 

 

2008-04-18 13:03:00     Re: change file wcfxs.c (si3210 driver)

Robin Getz (UNITED STATES)

Message: 54490    Hand:

 

>Is there anyone do it?

 

No

 

In fact, we are planning on removing the zaptel drivers (since they are not in mainline) and the astfin folks are maintaining/testing this - you might check over there.

 

-Robin

Attachments

    Outcomes