2008-04-17 06:20:44     How to choose output channels for AD1386A sound?

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-17 06:20:44     How to choose output channels for AD1386A sound?

Ihar Hrachyshka (BELARUS)

Message: 54406    Hello!

I build my BF533-EZKIT-based board sound system on AD1386A sound. One of my board's function is to play three different stereo sound streams simultaneously on it. What I done is choosing for AD1386 '3 stereos' option. After loading the kernel, my software is able to open pcm 3 times and plays sound properly, with no glitches or smth. The only missed functionality is that I can't specify the needed subdevice I want to play a stream on. I should have the possibility to play, f.e., mplayer stream on the 3rd stereo output while the 1st and the 2nd are not used. How can I do it?

Also that would be great if I can optionally play the same stream on all the outputs.

If I'm not wrong, this can be made through asound.conf settings though I can't figer out what are the right values. If I can choose next used output through kernel interface (kobject value or smth) then please tell me where should I look into.

 

Here are some info (line-in playing on the 1st subdevice):

 

root:~> aplay -l

**** List of PLAYBACK Hardware Devices ****

card 0: ad1836 [ADI ad1836], device 0: AD1836_PCM [AD1836_PCM]

Subdevices: 2/3

Subdevice #0: subdevice #0

Subdevice #1: subdevice #1

Subdevice #2: subdevice #2

 

root:~> cat /proc/asound/devices

0: [ 0] : control

16: [ 0- 0]: digital audio playback

24: [ 0- 0]: digital audio capture

33: : timer

 

root:~> cat /proc/asound/pcm

00-00: AD1836_PCM : AD1836_PCM : playback 3 : capture 1

 

root:~> cat /proc/asound/cards

0 [ad1836 ]: AD1836 - ADI ad1836

ADI ad1836 at PF4 SPORT0 rx/tx dma 1/2 err irq 10

 

root:~> cat /proc/asound/ad1836/registers

DAC_CTRL_1 0x0000

DAC_CTRL_2 0x1000

DAC_VOL_1L 0x23ff

DAC_VOL_1R 0x33ff

DAC_VOL_2L 0x43fa

DAC_VOL_2R 0x53fa

DAC_VOL_3L 0x63fa

DAC_VOL_3R 0x73fa

ADC_PEAK_1L 0xffff -63 dBFS

ADC_PEAK_1R 0xffff -63 dBFS

ADC_PEAK_2L 0xffff -63 dBFS

ADC_PEAK_2R 0xffff -63 dBFS

ADC_CTRL_1 0xc000

ADC_CTRL_2 0xd180

ADC_CTRL_3 0xe03a

 

root:~> cat /proc/asound/ad1836/pcm0p/info

card: 0

device: 0

subdevice: 0

stream: PLAYBACK

id: AD1836_PCM

name: AD1836_PCM

subname: subdevice #0

class: 0

subclass: 0

subdevices_count: 3

subdevices_avail: 2

 

root:~> ls /proc/asound/ad1836/pcm0p/

info oss sub0 sub1 sub2 xrun_debug

 

root:~> cat /proc/asound/ad1836/pcm0p/sub0/status

state: RUNNING

trigger_time: 1208611073.963748000

tstamp : 1208611991.506408000

delay : 6441

avail : 1751

avail_max : 6188

-----

hw_ptr : 44035799

appl_ptr : 44042240

 

root:~> cat /proc/asound/ad1836/pcm0p/sub1/status

closed

 

root:~> cat /proc/asound/ad1836/pcm0p/sub2/status

closed

 

Thanks for help.

QuoteReplyEditDelete

 

 

2008-04-17 15:14:05     Re: How to choose output channels for AD1386A sound?

Mike Frysinger (UNITED STATES)

Message: 54432    i think you would have to do it via alsa config files and options to mplayer ... you may have better luck asking on the mplayer or alsa mailing lists:

http://www.alsa-project.org/

http://www.mplayerhq.hu/

Attachments

    Outcomes