2008-04-09 06:42:47     kermit problem

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-09 06:42:47     kermit problem

Pranay Upadhyay (INDIA)

Message: 53907    Hello all,

  when I am sending the file using kermit on linux then I got the following error.

 

[root@PranayU ~]# cd /

[root@PranayU /]# kermit

?No keywords match - uImage.ext2

Command stack:

  1. File  : /root/.kermrc (line 10)

  0. Prompt: (top level)

C-Kermit 8.0.211, 10 Apr 2004, for Red Hat Linux 9.0

Copyright (C) 1985, 2004,

  Trustees of Columbia University in the City of New York.

Type ? or HELP for help.

Linux Kermit>  connect

Connecting to /dev/ttyS0, speed 57600

Escape character: Ctrl-\ (ASCII 28, FS): enabled

Type the escape character followed by C to get back,

or followed by ? to see other options.

----------------------------------------------------

 

(Back at PranayU)

----------------------------------------------------

Linux Kermit> send

?Filename required but not given

Linux Kermit> send uClinux.ext2

?File not found - "uClinux.ext2"

Linux Kermit> send /pranay/uClinux-dist/images/uImage.ext2

********************************************************************************************

C-Kermit 8.0.211, 10 Apr 2004, PranayU [192.168.0.127]

 

   Current Directory: /

Communication Device: /dev/ttyS0

Communication Speed: 57600

              Parity: none

         RTT/Timeout: 08 / 08

 

           File Type:

           File Size:

        Bytes So Far:

                          ...10...20...30...40...50...60...70...80...90..100

Estimated Time Left:

  Transfer Rate, CPS:

        Window Slots:

         Packet Type: S

        Packet Count: 1

       Packet Length: 28

         Error Count: 0

          Last Error:

        Last Message:

 

X to cancel file, Z to cancel group, <CR> to resend last packet,

E to send Error packet, ^C to quit immediately, ^L to refresh screen.

**************************************************************************************************

SEND-class command failed.

Packets sent: 2

Retransmissions: 11

Timeouts: 7

Damaged packets: 0

Fatal Kermit Protocol Error: Too many retries

 

HINTS... If the preceding error message does not explain the failure:

. Try changing the remote Kermit's FLOW-CONTROL setting.

. Adjust the timeout method (see HELP SET SEND).

. Increase the retry limit (see HELP SET RETRY).

. Try it again with SET STREAMING OFF.

. Try it again with SET PARITY SPACE.

. As a last resort, give a ROBUST command and try again.

Also:

. Be sure the source file has read permission.

. Be sure the target directory has write permission.

(Use SET HINTS OFF to suppress hints.)

*************************

  Please try to find solution early. I am not able to transfer the file from four to five days.And I am just working only on this.

    

                                    -Regards

                                       -Pranay

 

QuoteReplyEditDelete

 

 

2008-04-10 05:25:14     Re: kermit problem

Yi Li (CHINA)

Message: 54019    please follow: http://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:serial_port_loading_files&s[]=kermit

 

run "loadb" in uboot first.

QuoteReplyEditDelete

 

 

2008-04-12 07:31:08     Re: kermit problem

sathish kumar (HAITI)

Message: 54144   

 

Hi pranay,

 

can you explain the steps that you've carried out so that it would be helpful for me to sort out your problem.

 

How did you program the flash memory.

 

Are you using the serial cable that follows the instructions mentioned in blackfin.docs.

 

Explain the process in a stepwise manner.

 

regards

 

Sathish

Attachments

    Outcomes