2008-04-08 02:59:04     grep:.config:no such file or directory

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-04-08 02:59:04     grep:.config:no such file or directory

zhi shaolong (CHINA)

Message: 53808   

 

hi

 

when i configurate kernal,error "grep:.config:no such file or directory" exist.

 

and the window which is used to configurate the kernal has only two choises.(load an ...and save...),no vendor ..or kernal/defaule... as the document says.

 

can you tell me why?

 

thanks !

QuoteReplyEditDelete

 

 

2008-04-08 03:52:24     Re: grep:.config:no such file or directory

Yi Li (CHINA)

Message: 53810    Some files may be missing. Are you using SVN checkout or release package?

Please try again and post the full error message if still not working.

QuoteReplyEditDelete

 

 

2008-04-08 08:07:13     Re: grep:.config:no such file or directory

zhi shaolong (CHINA)

Message: 53838   

 

thank you!Yi Li

 

i am reading the SVN document now.

 

later i will tar the file again.

 

BTW ,are you chinese? do you have QQ?

 

maybe we can talk on QQ or MSN in chinese,more frequently.

 

my QQ:576150855

QuoteReplyEditDelete

 

 

2008-04-08 10:13:47     Re: grep:.config:no such file or directory

Mike Frysinger (UNITED STATES)

Message: 53843    then your configuration system is still not being generated properly under colinux

 

do:

rm config.in

make config.in

 

and post the output

QuoteReplyEditDelete

 

 

2008-04-08 22:52:38     Re: grep:.config:no such file or directory

zhi shaolong (CHINA)

Message: 53867   

 

thank you very much!

 

i have make this question out now.

Attachments

    Outcomes