2008-03-30 22:48:35     start uclinux error............

Document created by Aaronwu Employee on Aug 6, 2013
Version 1Show Document
  • View in full screen mode

2008-03-30 22:48:35     start uclinux error............

Bing Han (CHINA)

Message: 53341    when starting uclinux , it  stopped .

i use uclinux2008R1-Rc8.

Clock: VCO: 600 MHz, Core: 600 MHz, System: 120 MHz

SDRAM: 64 MB

FLASH:   8 MB

In:    serial

Out:   serial

Err:   serial

dm9000 i/o: 0x2c000000, id: 0x460a0090

Hit any key to stop autoboot:  0

## Booting image at 20100000 ...

   Image Name:   BF561 UCLINUX SYSTEM

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3347683 Bytes =  3.2 MB

   Load Address: 00040000

   Entry Point:  00040000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 40000  //stop here

 

why ?

TranslateQuoteReplyEditDelete

 

 

2008-03-30 23:05:58     Re: start uclinux error............

Yi Li (CHINA)

Message: 53342    how do you load your kernel? (tftp? please post the command).

What is uboot "bootargs" value?

QuoteReplyEditDelete

 

 

2008-03-31 16:07:46     Re: start uclinux error............

Robin Getz (UNITED STATES)

Message: 53391    Ice Cold:

 

Have a look at:

 

http://docs.blackfin.uclinux.org/doku.php?id=post_mortem

 

-Robin

QuoteReplyEditDelete

 

 

2008-04-01 00:54:44     Re: start uclinux error............

Bing Han (CHINA)

Message: 53400    thanks Robin for your  help

Attachments

    Outcomes