2008-03-19 04:50:44     The kgdb can't debug with adeos

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-03-19 04:50:44     The kgdb can't debug with adeos

new kernel (CHINA)

Message: 52745    I can debug driver in uClinuxR1-RC2 without adeos using kgdb normally .But I patch adeos in uclinux-RC2, i can 't debug by kgdb.

 

 

This is gdb :

 

(gdb) target remote udp:172.26.10.234:6443

Remote debugging using udp:172.26.10.234:6443

Ignoring packet error, continuing...

warning: unrecognized item "timeout" in "qSupported" response

Ignoring packet error, continuing...

Ignoring packet error, continuing...

Ignoring packet error, continuing...

Malformed response to offset query, timeout

 

 

This is booting information:

 

 

Starting Kernel at = 19c000

Linux version 2.6.22.16-ADI-2008R1-svn (josh@josh-laptop) (gcc version 4.1.2 (ADI svn)) #99 PREEMPT Wed Mar 19 16:18:59 CST 2008

Hardware Trace Off and Disabled

Warning: limiting memory to 15MB due to hardware anomaly 05000263

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 300 MHz core clock and 100 MHz System Clock

Board Memory: 16MB

Kernel Managed Memory: 16MB

Memory map:

  text      = 0x00001000-0x0013ecf0

  rodata    = 0x0013f000-0x00188b60

  data      = 0x00189000-0x0019c000

    stack   = 0x0018a000-0x0018c000

  init      = 0x0019c000-0x001ac000

  bss       = 0x001ac000-0x001ce640

  available = 0x001ce640-0x00eff000

  DMA Zone  = 0x00f00000-0x01000000

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 3802

Kernel command line: root=/dev/mtdblock2 rw rootfstype=jffs2 console=ttyBF0,115200 mtdparts=BF5xx-Flash:512k(uboot),1024k(kernel),15104k(jffs2) kgdboe=@172.26.10.234/,@172.26.10.115/

kgdboe: local port 6443

kgdboe: local IP 172.26.10.234

kgdboe: interface eth0

kgdboe: remote port 6442

kgdboe: remote IP 172.26.10.115

kgdboe: remote ethernet address ff:ff:ff:ff:ff:ff

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 64 (order: 6, 256 bytes)

I-pipe 1.7-00: pipeline enabled.

Dentry cache hash table entries: 2048 (order: 1, 8192 bytes)

Inode-cache hash table entries: 1024 (order: 0, 4096 bytes)

Memory available: 13156k/16384k RAM, (64k init code, 1271k kernel code, 510k data, 1024k dma, 360k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (16 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (42 KB free)

Security Framework v1.0.0 initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

Generic PHY: Registered new driver

NET: Registered protocol family 2

�IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 512 (order: 0, 4096 bytes)

TCP bind hash table entries: 512 (order: -1, 2048 bytes)

TCP: Hash tables configured (established 512 bind 512)

TCP reno registered

I-pipe: Domain Xenomai registered.

Xenomai: hal/blackfin started.

Xenomai: real-time nucleus v2.4.0 (Bells Of Lal) loaded.

Xenomai: starting native API services.

Xenomai: starting RTDM services.

JFFS2 version 2.2. © 2001-2006 Red Hat, Inc.

io scheduler noop registered (default)

 

FPGALoader Init major:250

 

fpgaregio Init

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 20) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

SMSC LAN83C185: Registered new driver

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac: Version 1.1, Blackfin BF53[67] BF527 on-chip Ethernet MAC driver

kgdboe: device eth0 not up yet, forcing it

kgdboe: carrier detect appears untrustworthy, waiting 4 seconds

PHY: 0:00 - Link is Up - 100/Full

kgdb: debugging over ethernet enabled

BF5xx flash: probing 16-bit flash bus

BF5xx-Flash: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

BF5xx-Flash: CFI does not contain boot bank location. Assuming top.

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

GHS FLASH was initalized already

Using static partition definition

Creating 3 MTD partitions on "BF5xx-Flash":

0x00000000-0x00080000 : "Bootloader"

0x00080000-0x00180000 : "Kernel1"

0x00180000-0x00e80000 : "JFFS2"

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

jffs2_scan_inode_node(): CRC failed on node at 0x0079b220: Read 0xffffffff, calculated 0xecbaa51a

VFS: Mounted root (jffs2 filesystem).

Freeing unused kernel memory: 64k freed

dma_alloc_init: dma_page @ 0x00294000 - 256 pages at 0x00f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.4.1 (2008-03-05 15:03:31 CST) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> ifconfig eth0 172.26.10.234

 

QuoteReplyEditDelete

 

 

2008-03-19 05:44:21     Re: The kgdb can't debug with adeos

Sonic Zhang (CHINA)

Message: 52749   

 

Adeos takes over all event entries from kernel. The kgdb exception may be ignored by ADEOS code. Changes are necessary to keep ADESO event entry code to work well with kgdb exception code.

 

 

QuoteReplyEditDelete

 

 

2008-03-26 08:21:54     Re: The kgdb can't debug with adeos

Paul Lau (UNITED STATES)

Message: 53050    Does it mean that once you patch the Kernel with ADEOS, you can no longer debug Kernel with KGDB. If that is the case, what are the alternatives to Kernel debugging. Would the Changes you mentioned be completed in the near future?

QuoteReplyEditDelete

 

 

2008-03-26 11:03:34     Re: The kgdb can't debug with adeos

Mike Frysinger (UNITED STATES)

Message: 53062    if you cant use the software solution of kgdb, then you need to use a jtag hardware solution in the meantime

QuoteReplyEditDelete

 

 

2008-03-27 03:48:16     Re: The kgdb can't debug with adeos

Yi Li (CHINA)

Message: 53100    Currently you may not debug adeos using KGDB. I am hoping this could be solved when kgdb is merged into mainline linux kernel (see: http://lwn.net/Articles/269378/) and upstream adeos will be updated accordingly.

 

For now, I think JTAG/gdbproxy could be used.

Attachments

    Outcomes