2008-03-23 20:16:26     How do I build an image suitable for the BF533-EZKIT eval board.

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-03-23 20:16:26     How do I build an image suitable for the BF533-EZKIT eval board.

Marshall Seaborn (UNITED STATES)

Message: 52946   

 

I've successfully built  uClinux-dist-2008R1-RC8 the images output is

 

as follows,

 

seaborn@123:~/Projects/uclinux-dist/images$ ls -al

total 30068

drwxr-xr-x  2 seaborn seaborn    4096 2008-03-23 11:25 .

drwxr-xr-x 17 seaborn seaborn    4096 2008-03-23 11:49 ..

lrwxrwxrwx  1 seaborn seaborn      18 2008-03-23 11:25 linux -> linux.initramfs.gz

-rwxr-xr-x  1 seaborn seaborn 7385804 2008-03-23 11:25 linux.initramfs

-rwxr-xr-x  1 seaborn seaborn 4637388 2008-03-23 11:25 linux.initramfs.gz

-rw-r--r--  1 seaborn seaborn 5440512 2008-03-23 11:24 rootfs.initramfs

-rw-r--r--  1 seaborn seaborn   18790 2008-03-23 11:24 rootfs.initramfs.contents

-rw-r--r--  1 seaborn seaborn 2689215 2008-03-23 11:24 rootfs.initramfs.gz

-rw-r--r--  1 seaborn seaborn  426886 2008-03-23 11:25 System.map.initramfs

-rw-r--r--  1 seaborn seaborn  426886 2008-03-23 11:25 System.map.initramfs.gz

lrwxrwxrwx  1 seaborn seaborn      16 2008-03-23 11:25 uImage -> uImage.initramfs

-rw-r--r--  1 seaborn seaborn 3477950 2008-03-23 11:25 uImage.initramfs

-rw-r--r--  1 seaborn seaborn 3462730 2008-03-23 11:25 uImage.initramfs.gz

-rw-r--r--  1 seaborn seaborn  786633 2008-03-23 11:24 vmImage

-rwxr-xr-x  1 seaborn seaborn 1930885 2008-03-23 11:24 vmlinux

 

How do I build an image for the ADI BF533-EZKIT Eval board?  Is there documentation that will

 

explain the process?

 

 

 

Thanks for your reply,

 

Marshall

QuoteReplyEditDelete

 

 

2008-03-23 20:35:28     Re: How do I build an image suitable for the BF533-EZKIT eval board.

Mike Frysinger (UNITED STATES)

Message: 52947    just boot the uImage like normal

Attachments

    Outcomes