2008-02-20 03:00:16     Problems Building Konqueror

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-20 03:00:16     Problems Building Konqueror

xabi romero (UNITED STATES)

Message: 51313    I am trying to build the konqueror web browser using the latest svn toolchain and uclinux-distr.

when i do "make" i obtaine the following error (see the attached file).

I have the qt library working and i and trying to build FDPIC konqueror with shared QT library

 

-Xabi

konqueror_make_error

QuoteReplyEditDelete

 

 

2008-02-20 11:17:38     Re: Problems Building Konqueror

Robin Getz (UNITED STATES)

Message: 51363    Xabi:

 

I think you might have better luck with the 2008R1 branches than using trunk.

 

-Robin

QuoteReplyEditDelete

 

 

2008-02-21 02:53:24     Re: Problems Building Konqueror

xabi romero (UNITED STATES)

Message: 51405   

 

Thanks Robin

 

When you tell me that i might to use the 2008R1 branches, is for the Toolchain or for kernel + toolchain+distro.

 

thanks

 

-Xabi

QuoteReplyEditDelete

 

 

2008-02-21 03:03:17     Re: Problems Building Konqueror

Mike Frysinger (UNITED STATES)

Message: 51406    please review the FAQ about different versions:

http://docs.blackfin.uclinux.org/doku.php?id=faq

QuoteReplyEditDelete

 

 

2008-02-27 06:33:32     Re: Problems Building Konqueror

xabi romero (UNITED STATES)

Message: 51730   

 

I am a new developper in uClinux, and i need more help.

 

Do anybody have problems building the konqueror explorer?

 

if somebody have build it, with wich toolchain, distribution and kernel?

 

thanks again.

QuoteReplyEditDelete

 

 

2008-02-27 11:08:13     Re: Problems Building Konqueror

Robin Getz (UNITED STATES)

Message: 51745    Xabi:

 

Have a look at:

 

http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:browsers&s=konq#konqueror3_embedded

 

It should work with the 2008R1 toolchain and dist. If it doesn't, it is a bug (either in the docs, or in the source) - let us know, and we can fix either.

 

-Robin

QuoteReplyEditDelete

 

 

2008-02-28 02:45:57     Re: Problems Building Konqueror

xabi romero (UNITED STATES)

Message: 51760   

 

Ok. i a going to try with the 2008R1 version.

 

The problem that i had, was maken with the latest svn dist. and toolchain, and i follow the documentation.

 

Thanks

 

-Xabi

QuoteReplyEditDelete

 

 

2008-03-04 11:37:29     Re: Problems Building Konqueror

xabi romero (UNITED STATES)

Message: 52036   

 

Finally i download the2008R1 branches from kernel, uclinux and toolcahin, and when i try to make , i have obtained the same error (as you can see in the first message)

 

Do anybody try to compile the konqueror web browser?

 

thanks

 

-Xabi

QuoteReplyEditDelete

 

 

2008-03-13 10:02:26     Re: Problems Building Konqueror

Robin Getz (UNITED STATES)

Message: 52454    Xabi:

 

Sonic has done it, but I don't think updated things in awhile.

 

I think Mike was looking at integrating both Qt and Konqueror into trunk.

 

-Robin

Attachments

Outcomes