2007-12-13 08:07:18     build error - segmentation error

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2007-12-13 08:07:18     build error - segmentation error

Peter Nielsen (DENMARK)

Message: 48563    Hello

 

I have made a complete new installation on a new PC.

I am using 2007R1-RC3 release (gnu toolchain, linux kernel, uclinux)

 

I select BF537 all other settings is default.

But i get an Segmentation error at ext2 fs generation

 

 

I tried to increase  to 16 and 20MB (INODE1024) and with 12mb  (INODE 2048)

 

 

But i will not build - i allway get an:

 

Segmentation fault      bfin-uclinux-genext2fs

 

other fs is made as you can see from added file.

 

Does anyone have clue what is wrong

 

-peter

new file

QuoteReplyEditDelete

 

 

2007-12-13 14:04:08     Re: build error - segmentation error

Mike Frysinger (UNITED STATES)

Message: 48569    what version of glibc do you have ?  run:

/lib/libc.so.6

on your development system

QuoteReplyEditDelete

 

 

2007-12-14 01:24:35     Re: build error - segmentation error

Peter Nielsen (DENMARK)

Message: 48579    Hi Mike

 

I am using the relatively new FEDORA8 release on my development PC

 

[root@localhost lib]# ./libc.so.6

GNU C Library stable release version 2.7, by Roland McGrath et al.

Copyright (C) 2007 Free Software Foundation, Inc.

This is free software; see the source for copying conditions.

There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A

PARTICULAR PURPOSE.

Compiled by GNU CC version 4.1.2 20070925 (Red Hat 4.1.2-32).

Compiled on a Linux >>2.6.20-1.3001.fc6xen<< system on 2007-10-18.

Available extensions:

        The C stubs add-on version 2.1.2.

        crypt add-on version 2.1 by Michael Glad and others

        GNU Libidn by Simon Josefsson

        Native POSIX Threads Library by Ulrich Drepper et al

        BIND-8.2.3-T5B

        RT using linux kernel aio

For bug reporting instructions, please see:

<http://www.gnu.org/software/libc/bugs.html>.

[root@localhost lib]#

 

 

Does above give you a clue what could be wrong.

 

-Peter

QuoteReplyEditDelete

 

 

2007-12-14 01:33:32     Re: build error - segmentation error

Mike Frysinger (UNITED STATES)

Message: 48580    you're hitting a bug in glibc-2.7

 

your choices:

- bug the fedora guys to fix it

- upgrade your install

- use an older distro

- fix it yourself

- dont use EXT2 romfs

QuoteReplyEditDelete

 

 

2007-12-14 03:28:26     Re: build error - segmentation error

Peter Nielsen (DENMARK)

Message: 48581   

 

Hi Mike

 

Thanks for the quick reply

 

I will go back to FEDORA 7 version.

 

-Peter

QuoteReplyEditDelete

 

 

2007-12-17 08:52:11     Re: build error - segmentation error

Greg Wingfield (UNITED KINGDOM)

Message: 48642    Thanks for the info, I had exactly the same problem. I have now downgraded to Fedora 7 and all is working fine 8-)

QuoteReplyEditDelete

 

 

2007-12-17 14:34:19     Re: build error - segmentation error

Mike Frysinger (UNITED STATES)

Message: 48657    the issue has been fixed in upstream glibc, but i have no idea when the Fedora system will see that fix

QuoteReplyEditDelete

 

 

2008-02-25 14:03:26     Re: build error - segmentation error

Alexey Novgorodov (RUSSIAN FEDERATION)

Message: 51614    please tell me what is ID of this bug in libc bugzilla

 

i am using ubuntu, and it seems that this bug will  not be fixed shortly. so i need to patch libc sources manually

QuoteReplyEditDelete

 

 

2008-02-25 14:47:51     Re: build error - segmentation error

Mike Frysinger (UNITED STATES)

Message: 51618    please read the FAQ:

http://docs.blackfin.uclinux.org/doku.php?id=faq

Attachments

Outcomes