2008-02-22 11:18:42     Accessing/mounting HD (EZkit bf548, recent trunk): system hangs

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-22 11:18:42     Accessing/mounting HD (EZkit bf548, recent trunk): system hangs

Piggebu Piggebu (ANDORRA)

Message: 51507    Hi all

 

With a recent trunk (some weeks ago) I have the problem that the system hangs if I try to access the hard disk (40GB) on the EZ-Kit BF548 Board. I can mount it but as soon as I try to access it (for ex: ls [mountpath]) the system hangs.

 

 

All worked fine with an older trunk (late Dezember 07).

 

When I mount it, it gives me the following warning (also with the old trunk):

root:~> mount /dev/sda1 home/devel/HD/

EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended

root:~>

 

When I try to do a e2fsck:

- with the old trunk: the following error trace is printed: see e2fsck_log.txt

- with the new trunk: the system hangs, I let it run for some 2 or 3 hours, no message was printed..

 

I am not sure if running e2fsck will solve the problem of the hanging system when accessing the mounted HD... but its the only trace for now (?)

 

Thanks for any advice

Regards

Piggebu

e2fsck_log.txt

QuoteReplyEditDelete

 

 

2008-02-22 11:48:43     Re: Accessing/mounting HD (EZkit bf548, recent trunk): system hangs

Michael Hennerich (GERMANY)

Message: 51510   

 

Can you try to comment out this line in

 

vendors/AnalogDevices/BF548-EZKIT/Makefile

 

# $(ROMFSINST) -e CONFIG_PATA_BF54X -a "echo 20 > /proc/sys/vm/pagecache_ratio" /etc/rc

 

and see if this makes a difference?

 

-Michael

QuoteReplyEditDelete

 

 

2008-02-25 03:34:57     Re: Accessing/mounting HD (EZkit bf548, recent trunk): system hangs

Piggebu Piggebu (ANDORRA)

Message: 51581    ....and here we go!! :-)

 

Thank you very much Michael! Everything works now, all little spooky things are gone (i.e. fine) as well (strange command prompt, accessing HD, working libusb etcetc)!

 

*uff* finally

Thanks again and kind regards

Piggebu

Attachments

Outcomes