2008-02-19 17:54:52     ADC/DAC versus CODEC

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-19 17:54:52     ADC/DAC versus CODEC

Jan Kowalski (POLAND)

Message: 51299   

 

Hi,

 

As we known AD1836A Audio Daughter Board  will be availabe late April'08, ADC are availabe now and DAC will be availabe in few days.

 

Q.

 

Can we use from hardware view (connection to STAMP) and from software view 2 cards ADC&DAC together to simulate CODEC?

 

Please advise.

 

Maybe you have other solution?

 

Regards

 

M

QuoteReplyEditDelete

 

 

2008-02-20 11:42:49     Re: ADC/DAC versus CODEC

Robin Getz (UNITED STATES)

Message: 51367    Marek:

 

I'm not sure I understand the question?

 

You want to design your own card? or use the parts on a different one?

 

-Robin

QuoteReplyEditDelete

 

 

2008-02-20 11:51:38     Re: ADC/DAC versus CODEC

Jan Kowalski (POLAND)

Message: 51369   

 

Hi,

 

No I do not want to design my own card, I am to much delay with my stuff to do it.

 

I thought, maybe someone have one spare I can PO.

 

Today I received update from AD Customer Support , and in real life I could have this card with me in late June. It is to long.

 

 

 

Regards

 

M2007-10-04 10:32:18     Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 44905   

Hi all,

 

I develop a board with a bf537. On this board, I have :

- One stereo amplifier (to output sound on speakers)

- One stereo line output jack

- One mono amplifier (to output sound on another speaker)

- One stereo line input jack

- One mono mike input jack

- One stereo FM tuner (on the board)

 

The usage of the board follows :

 

- The mono ouptut must be independant (his only usage is to play mono audio files)

 

- The stereo output is done on the stereo amplifier OR the stereo line output jack (to use an external amplifier)

 

On this stereo output, I need to :

 

- Play audio files (In this case inputs are not used)

- Play the FM

- Play the sound from the line

- Play the sound from the mike

 

In other word, in all cases there is only one input to sample (Line in, FM, or mike), and the mono output must be independant.

 

Do you think it's possible to do that with the AD1981B ? How must I connect the differents peripherals on the codec ?

 

My idea is :

 

- Stereo amplifier connected on HP_OUT_R and HP_OUT_L

- Stereo line out connected on LINE_OUT_R and LINE_OUT_L

- Mono amplifier connected on MONO_OUT

- Stereo line input connected on LINE_IN_R and LINE_IN_L

- FM tuner connected on AUX_R and AUX_L

- Mike connected on MIC1

 

What do you think about this ?

 

Thank you and best regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-10-04 11:41:36     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 44914    Cyril:

 

I'm not clear what you want to do.

 

There is only one set of DACs, and one set of ADCs on the AD1981BL. You can do some things with the hardware mixer (see the datasheet of the AD1981), but when you say that mono out must be independant - what do you mean?

 

Thanks

-Robin

QuoteReplyEditDelete

 

 

2007-10-04 13:11:00     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 44928    Yes your are right, the codec is not good for what I want to do. I need the AD1980 but it doesn't exist in industrial version (-40 / +70°c).

 

For the mono output, I mean that it must be independant. It fact, I need 2 independant channel.

 

For exemple, I need to play a file on the mono output, and play another file (or FM, or Mike, or line in) on the stereo output.

 

I am searching for a codec, in industrial version.

Thus the minimum I need is 4 DAC ( 2 stereo output, I can use one to do mono), and 2 ADC.

 

The AD1986 seems to be OK (6 DAC / 2 ADC), with industrial version.

 

Thanks,

CYril

TranslateQuoteReplyEditDelete

 

 

2007-10-04 14:25:19     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 44938    Cyril:

 

I might stick with the AD1986A -

http://www.analog.com/en/prod/0,2877,AD1986A,00.html

 

I think it meets your requirements:

- 6 DAC

- 2 ADC

- -40 to 85C

- slot16 mode

 

I just need to check with one of our developers - to make sure you can use it before you lay out a board.

 

The Blackfin does not include real AC'97 controller it is a little tricky to use these parts, and I don't think anyone has done a 6 channel output yet.

 

-Robin

QuoteReplyEditDelete

 

 

2007-10-04 15:22:07     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 44940    I just need 2 channels, one channel will be unused.

 

I saw in the kernel config that the AD1836 can work in 5.1 or 3 separate stereo channel. In fact the /dev/dsp can be opened 3 time to access the 3 separate channel.

 

These 2 parts are very different to manage ?

 

Thanks,

Regards

TranslateQuoteReplyEditDelete

 

 

2007-10-04 20:38:59     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 44948    Cyril:

 

Yes - AD1836 is nothing like the AD1986.

 

One is designed to be used on the SPORT, and the AC 97 codecs are not.

 

-Robin

QuoteReplyEditDelete

 

 

2007-10-05 04:24:49     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 44956    Hi Robin,

 

Yesterday evening I looked in the sound/blackfin/ac97_sport.c.

 

This source seem's to be very clean, and permit to transfer AC97 frame over the SPORT ?

If I understand, every "sample" consist on a "ac97_frame" data structure. I can see that this structure contain a lot of pad word, and only contain one PCM data word.

 

It seem's to be logical because this file is used by ad1981b.c, which just have one stereo channel.

 

For other codec with more channels, as the AD1986A, maybe "I have just" to add another PCM data word in the ac97_frame ? Like this :

 

struct ac97_frame {

        __u16 ac97_tag;         // slot 0

        __u16 ac97_addr;        // slot 1

        __u16 ac97_data;        // slot 2

        __u32 ac97_pcm1;         // slot 3 and 4: left and right pcm data for 1st DAC

        __u32 ac97_pcm2;         // slot 5 and 6: left and right pcm data for 2nd DAC

        __u16 stuff[9];        // pad to 16 words

} __attribute__ ((packed));

 

If the ac97 data transfer for multiple channel work like this, after I need to modify the source to have access to this 2nd pcm data as an independant channel :-/

TranslateQuoteReplyEditDelete

 

 

2007-10-05 05:34:42     Re: Advanced usage of the AD1981B codec

Michael Hennerich (GERMANY)

Message: 44959    Cyril,

 

all Sound Codecs sit on the SPORT.

You are better off using a AC97 Codec.

(it allows you to mix analog inputs with the output be just setting a register)

have a look into the datasheet

 

On SVN trunk there is a new Blackfin ASOC driver for AC97 codecs.

This new driver will or already does support multiple channels.

We support the AD1980 and AD1981 and I'm pretty sure the AD1986 will also work - with only one line changed in the driver.

 

The driver you are refering to has been deleted by me - and will no longer be released.

 

-Michael

QuoteReplyEditDelete

 

 

2007-10-05 07:48:15     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 44968    Michael,

 

Thank you very much for your answer.

 

What you say is a very good new for me. I think I can mount the AD1986A on board without risk.

AC97 codec is good for me because I don't need to have a spi or i2c connection to configure the codec. On my board I dedicated the SPI to sample some ADC, and I don't want other peripheral on it. And I dedicated the i2c to control the FM tuner only, because the Fm tuner need no activity on i2c when seeking for optimal performance.

 

And you are right, I have seen that I can mix input with the output. It's perfect for my needs because I can play the line input, FM, or mike input directly on the stereo output without read / write samples in software.

And I think I can easily choose where to send the stereo output, on the stereo amplifier or on the line output.

 

And I channels can be independant, I will be able to have my mono output independant.

 

Regards

TranslateQuoteReplyEditDelete

 

 

2007-10-05 14:54:54     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 44989    Cyril:

 

Transferring  the data to/from the DAC/ADCs is not the problem - it is getting access to all the registers properly to set up/control the mixer functionality.

 

I need to check if this is doable before you design hardware.

 

Last time I talked to Michael about the required programming sequence for startup on the codecs - we determined it was pretty difficult.

 

-Robin

QuoteReplyEditDelete

 

 

2007-10-05 17:07:53     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 45006    There is a big difference between the ad1981 and ad1986 for accessing register ?

I have not looked in detail the ac97 specification, but it seems the register is acceded with the three first word of each sample frame ?

I like to know how things work, can you rapidly explain what is your concern ?

 

Thank your for your help.

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-10-10 11:06:23     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 45186    Hi Robin,

 

Have you a good new for me ?

 

I have no other choice, I must put the AD1986A in my hardware. There is no other codec which can do what I want to do.

Thus I implement the AD1986A, and I pray to have a working driver, even if I must modify it.

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-10-22 13:05:36     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 45754    Cyril:

 

Sorry for the delay.

 

The problem is that the SPORT is not an AC'97 controller. Using a codec that supports Slot 16 mode is possible, but it is error prone.

 

-Robin

QuoteReplyEditDelete

 

 

2007-12-21 19:23:04     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 48910    Hi robin and Michael,

 

I reread all messages of this thread.

Michael you say that it's better to use an AC97 codec, and that there is no problem with the blackfin SPORT, and Robin you say it will very difficult to have the AD1968A working. What is the truth !? :))))

 

On my side I had no other solution, so I implanted the AD1968A on my board (you can see it on the image...). Thus it must works, and it will works !

 

<meta content="text/html; charset=UTF-8" http-equiv="Content-Type" />Michael, 2 day ago you said on the SVN trunk is a new blackfin ASOC driver for AC97 codec.

I work on the last SVN trunk but I don't see what you talk about. What is "ASOC" ? Can you tell me where is the driver ?

 

Regards,

Cyril

dsc05167.jpg

TranslateQuoteReplyEditDelete

 

 

2007-12-22 18:17:07     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 48917    Cyril:

 

We are both right.

 

In simple audio cases - it will work fine.

 

In more complicated audio cases (mixing, VOIP, etc) we are still struggling with it.

 

ASOC == ALSA System on a Chip

 

-Robin

QuoteReplyEditDelete

 

 

2007-12-22 18:33:09     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 48918    Hi robin.

 

In my case I have no complicated usage, I wich :

- 2 indepedant channels (the 3th is unused), one stereo, one mono (or stereo too, I mix the 2 channels in hardware)

- On the mono output, I just need to play audio file (wav, mp3...)

- On the stereo output, I need to play audio file (wav, mp3), or play sound from line input or AUX input.

 

Where can I find the AC97 codec than Michael was talking about ?

I am interested to look at it, to understand how works sound layer, and begin to work with it.

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-12-22 18:38:53     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 48919    It's OK, I have found it. Your explanation for ASOC helped me to found it

 

linux-2.6.x/sound/soc/blackfin

 

I look at the code.

TranslateQuoteReplyEditDelete

 

 

2007-12-23 00:27:44     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 48921    Cyril:

 

Do you need software mixing? I can't understand from your description. If so - today that does not work, although we are working on fixing it.

 

You can find the audio device - the same place you find all the other audio device - Linux -> Device Drivers -> Sound

QuoteReplyEditDelete

 

 

2007-12-23 09:49:57     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 48924    No, I think I don't need software mixing.

I try to detail my need :

 

Inputs on the codec are :

- Mike input (connected on MIC1)

- An FM tuner (connected on LINE_IN_R and LINE_IN_L )

- An AUX in jack (connected on AUX_R and AUX_L)

 

Outputs on the codec are :

- Class D mono amplifier (connected on SURR_OUT_R and SURR_OUT_L, mixed on hardware to have mono, even if a stereo file is played).

- Class D stereo amplifier (connected on LINE_OUT_R and LINE_OUT_L)

- Aux OUT jack (connected on HP_OUT_R and HP_OUT_L)

 

 

On the mono output (SURR_OUT_R, SURR_OUT_L), I just need to play audio files.

 

On the stereo output OR aux. output jack (if external amplifier is connected, or head phone), I need to :

- Play audio file

or

- Play the FM tuner

or

- Play the AUX in jack

 

In the future, I will need to record the mike input, but not necessary for now.

 

Does I need software mixing to do that ? I think not ? On the outputs I never have more than one audio source to play.

 

Futhermore, with the AC97, it seem's that to play the FM tuner input on the stereo output or the aux. output jack, it's just a register configuration in the AD1986A to do hardware mixing. Same thing to play the AUX in jack on the stereo output or the AUX. output jack.

 

Do you understand what I need to do ? It's true my english is not perfect, it's not easy to explain

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-12-26 05:55:20     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 48970    Hi all,

 

I activated ALSA for soc audio support, SOC audio for the ADI BF5xx chip, and SoC AC97 audio support for BF5xx.

As AD1986 and AD1980 are similar, to test purpose I also modified linux-2.6.x/sound/soc/codecs/ad1980.c :

 

        //if (vendor_id2 != 0x5370) {

        if (vendor_id2 != 0x5378) {

                if (vendor_id2 != 0x5374)

                        goto reset_err;

                else

                        printk(KERN_WARNING "ad1980: "

                                "Found AD1981 - only 2/2 IN/OUT Channels "

                                "supported\n");

        }

 

When I boot I have :

 

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

ASoC version 0.13.1

AD1980 SoC Audio Codec

dma_alloc_init: dma_page @ 0x03403000 - 256 pages at 0x03f00000

asoc: AC97 <-> bf5xx-ac97 mapping ok

Vendor ID 1 : 4144

Vendor ID 2 : 5378

ALSA device list:

  #0: bf5xx-board (AD1980)

 

I put debug to print the Vendor's IDs and verify that communication is OK with the codec. Everyting seems to be OK.

 

Some files in /proc :

 

root:~> ls -l /proc/asound/

lrwxrwxrwx    1 root     root            5 Jan  1 00:16 bf5xxboard -> card0

dr-xr-xr-x    4 root     root            0 Jan  1 00:16 card0

-r--r--r--    1 root     root            0 Jan  1 00:16 cards

-r--r--r--    1 root     root            0 Jan  1 00:16 devices

dr-xr-xr-x    2 root     root            0 Jan  1 00:16 oss

-r--r--r--    1 root     root            0 Jan  1 00:16 pcm

-r--r--r--    1 root     root            0 Jan  1 00:16 timers

-r--r--r--    1 root     root            0 Jan  1 00:16 version

 

root:~> ls -l /proc/asound/card0/

-r--r--r--    1 root     root            0 Jan  1 00:18 id

-rw-r--r--    1 root     root            0 Jan  1 00:18 oss_mixer

dr-xr-xr-x    3 root     root            0 Jan  1 00:18 pcm0c

dr-xr-xr-x    3 root     root            0 Jan  1 00:18 pcm0p

 

root:~> cat /proc/asound/devices

  0: [ 0]   : control

16: [ 0- 0]: digital audio playback

24: [ 0- 0]: digital audio capture

33:        : timer

 

root:~> cat /proc/asound/cards

0 [bf5xxboard     ]: AD1980 - bf5xx-board

                      bf5xx-board (AD1980)

 

The problem is that I don't have any /dev/dsp device, thus when I test tone, for example :

 

root:~> tone

ERROR: failed to open DAC device /dev/dsp

 

Do I forget to do something ?

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-12-26 07:34:46     Re: Advanced usage of the AD1981B codec

Mike Frysinger (UNITED STATES)

Message: 49016    tone does not use alsa, it uses oss ... so if you didnt enable/load the oss emulation layer, it isnt going to work

QuoteReplyEditDelete

 

 

2007-12-26 08:02:32     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49017    Yet, I have activated the oss layer in my kernel config :

 

OSS mixer API : activated

OSS PCM API (digital audio) : activated

OSS PCM API (digital audio), include plugin system : activated

 

But /dev/dsp doesn't exist

TranslateQuoteReplyEditDelete

 

 

2007-12-26 14:27:04     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 49019    Cyril:

 

I don't know - you may want to check if your system needs to have the hard reset?

 

This is what my working system looks like:

 

root:/usr/bin> ls -lR /proc/asound/

/proc/asound/:

lrwxrwxrwx    1 root     root            5 Dec 11 11:52 bf5xxboard -> card0

dr-xr-xr-x    4 root     root            0 Dec 11 11:52 card0

-r--r--r--    1 root     root            0 Dec 11 11:52 cards

-r--r--r--    1 root     root            0 Dec 11 11:52 devices

dr-xr-xr-x    2 root     root            0 Dec 11 11:52 oss

-r--r--r--    1 root     root            0 Dec 11 11:52 pcm

-r--r--r--    1 root     root            0 Dec 11 11:52 timers

-r--r--r--    1 root     root            0 Dec 11 11:52 version

 

/proc/asound/card0:

-r--r--r--    1 root     root            0 Dec 11 11:52 id

-rw-r--r--    1 root     root            0 Dec 11 11:52 oss_mixer

dr-xr-xr-x    3 root     root            0 Dec 11 11:52 pcm0c

dr-xr-xr-x    3 root     root            0 Dec 11 11:52 pcm0p

 

/proc/asound/card0/pcm0c:

-r--r--r--    1 root     root            0 Dec 11 11:52 info

-rw-r--r--    1 root     root            0 Dec 11 11:52 oss

dr-xr-xr-x    2 root     root            0 Dec 11 11:52 sub0

 

/proc/asound/card0/pcm0c/sub0:

-r--r--r--    1 root     root            0 Dec 11 11:52 hw_params

-r--r--r--    1 root     root            0 Dec 11 11:52 info

-r--r--r--    1 root     root            0 Dec 11 11:52 status

-r--r--r--    1 root     root            0 Dec 11 11:52 sw_params

 

/proc/asound/card0/pcm0p:

-r--r--r--    1 root     root            0 Dec 11 11:52 info

-rw-r--r--    1 root     root            0 Dec 11 11:52 oss

dr-xr-xr-x    2 root     root            0 Dec 11 11:52 sub0

 

/proc/asound/card0/pcm0p/sub0:

-r--r--r--    1 root     root            0 Dec 11 11:52 hw_params

-r--r--r--    1 root     root            0 Dec 11 11:52 info

-r--r--r--    1 root     root            0 Dec 11 11:52 status

-r--r--r--    1 root     root            0 Dec 11 11:52 sw_params

 

/proc/asound/oss:

-r--r--r--    1 root     root            0 Dec 11 11:52 devices

-r--r--r--    1 root     root            0 Dec 11 11:52 sndstat

 

This might be more important:

 

root:/usr/bin> ls -lR /sys/devices/platform/soc-audio/

/sys/devices/platform/soc-audio/:

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 bus -> ../../../bus/platform

-r--r--r--    1 root     root         4096 Dec 11 11:53 codec_reg

-r--r--r--    1 root     root         4096 Dec 11 11:53 dapm_widget

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 driver -> ../../../bus/platform/drivers/soc-audio

-r--r--r--    1 root     root         4096 Dec 11 11:53 modalias

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 sound:audio -> ../../../class/sound/audio

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 sound:controlC0 -> ../../../class/sound/controlC0

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 sound:dsp -> ../../../class/sound/dsp

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 sound:mixer -> ../../../class/sound/mixer

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 sound:pcmC0D0c -> ../../../class/sound/pcmC0D0c

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 sound:pcmC0D0p -> ../../../class/sound/pcmC0D0p

lrwxrwxrwx    1 root     root            0 Dec 11 11:53 subsystem -> ../../../bus/platform

-rw-r--r--    1 root     root         4096 Dec 11 11:53 uevent

root:/usr/bin>

 

root:/usr/bin> cat /sys/devices/platform/soc-audio/codec_reg

AD1980 registers

0:   90

2:    0

4: 8000

6: 8000

8:    0

a:    0

c: 8008

e: 8008

10: 8808

12: 8808

14:    0

16: 8808

18:    0

1a:    0

1c:    0

1e:    0

20:    0

22:    0

24:    0

26:    f

28:  3c7

2a:  1f0

2c: bb80

2e: bb80

30: bb80

32: bb80

34:    0

36: 8080

38: 8080

3a: 2000

3c:    0

3e:    0

40:    0

42:    0

44:    0

46:    0

48:    0

4a:    0

4c:    0

4e:    0

50:    0

52:    0

54:    0

56:    0

58:    0

5a:    0

5c:    0

5e:    0

60: 8080

62:    0

64:    0

66:    0

68:    0

6a:    0

6c:    0

6e:    0

70:    0

72:    0

74: 9900

76:    0

78:    0

7a:    0

7c: 4144

7e: 5370

 

root:/usr/bin> ls /dev/dsp -l

crw-rw----    1 root     root      14,   3 Dec 11 11:30 /dev/dsp

 

 

Does it work if you just create the /dev/dsp by hand?

 

-Robin

QuoteReplyEditDelete

 

 

2007-12-26 15:30:34     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49020    Robin, I will check tomorrow morning, but from my memory, I have exactly the sames outputs for proc/asound/...

I have not checked the /sys/devices/platform/soc-audio, but I am pretty sure it will be OK, I check that tomorrow morning.

 

On your system, have you a /dev/sound directory ? Because I looked on internet, /dev/dsp is for OSS, alsa device are in /dev/sound apparently (it's true on my laptop).

 

But I think to something : do I need to install alsalib to see the sound device in /dev ?

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-12-26 20:14:23     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 49021    Cyril:

 

You should not have /dev/sound, but /dev/snd/

 

root:~> ls -l /dev/snd/

crw-rw-r--    1 root     root     116,   0 Dec 11 17:41 controlC0

crw-rw-r--    1 root     root     116,  24 Dec 11 17:41 pcmC0D0c

crw-rw-r--    1 root     root     116,  16 Dec 11 17:41 pcmC0D0p

crw-rw-r--    1 root     root     116,  33 Dec 11 17:41 timer

 

-Robin

QuoteReplyEditDelete

 

 

2007-12-27 04:41:51     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49032    Hi Robin,

 

I have not exactly the same output as you :

 

root:~> ls -lR /proc/asound/

/proc/asound/:

lrwxrwxrwx    1 root     root            5 Jan  1 00:00 bf5xxboard -> card0

dr-xr-xr-x    2 root     root            0 Jan  1 00:00 card0

-r--r--r--    1 root     root            0 Jan  1 00:00 cards

-r--r--r--    1 root     root            0 Jan  1 00:00 devices

dr-xr-xr-x    2 root     root            0 Jan  1 00:00 oss

-r--r--r--    1 root     root            0 Jan  1 00:00 pcm

-r--r--r--    1 root     root            0 Jan  1 00:00 timers

-r--r--r--    1 root     root            0 Jan  1 00:00 version

 

/proc/asound/card0:

-r--r--r--    1 root     root            0 Jan  1 00:00 id

-rw-r--r--    1 root     root            0 Jan  1 00:00 oss_mixer

 

/proc/asound/oss:

-r--r--r--    1 root     root            0 Jan  1 00:00 devices

-r--r--r--    1 root     root            0 Jan  1 00:00 sndstat

root:~>

 

 

 

 

root:~> ls -lR /sys/devices/platform/soc-audio/

/sys/devices/platform/soc-audio/:

-r--r--r--    1 root     root         4096 Jan  1 00:01 codec_reg

-r--r--r--    1 root     root         4096 Jan  1 00:01 dapm_widget

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 driver -> ../../../bus/platform/drivers/soc-audio

-r--r--r--    1 system -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

root:~> rwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../bus/platform

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound:

drwxr-xr-x    8 root     root            0 Jan  1 00:00 card0

 

/sys/devices/platform/soc-audio/sound/card0:

drwxr-xr-x    2 root     root            0 Jan  1 00:00 audio

drwxr-xr-x    2 root     root            0 Jan  1 00:00 controlC0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../devices/platform/soc-audio

drwxr-xr-x    2 root     root            0 Jan  1 00:00 dsp

drwxr-xr-x    2 root     root            0 Jan  1 00:00 mixer

drwxr-xr-x    2 root     root            0 Jan  1 00:00 pcmC0D0c

drwxr-xr-x    2 root     root            0 Jan  1 00:00 pcmC0D0p

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound/card0/audio:

-r--r--r--    1 root     root         4096 Jan  1 00:01 dev

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../../devices/platform/soc-audio/sound/card0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound/card0/controlC0:

-r--r--r--    1 root     root         4096 Jan  1 00:01 dev

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../../devices/platform/soc-audio/sound/card0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound/card0/dsp:

-r--r--r--    1 root     root         4096 Jan  1 00:01 dev

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../../devices/platform/soc-audio/sound/card0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound/card0/mixer:

-r--r--r--    1 root     root         4096 Jan  1 00:01 dev

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../../devices/platform/soc-audio/sound/card0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound/card0/pcmC0D0c:

-r--r--r--    1 root     root         4096 Jan  1 00:01 dev

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../../devices/platform/soc-audio/sound/card0

-r--r--r--    1 root     root         4096 Jan  1 00:01 pcm_class

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

 

/sys/devices/platform/soc-audio/sound/card0/pcmC0D0p:

-r--r--r--    1 root     root         4096 Jan  1 00:01 dev

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 device -> ../../../../../../devices/platform/soc-audio/sound/card0

-r--r--r--    1 root     root         4096 Jan  1 00:01 pcm_class

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 subsystem -> ../../../../../../class/sound

-rw-r--r--    1 root     root         4096 Jan  1 00:01 uevent

root:~>

 

 

All this is with ALSA for SoC audio support, SoC Audio for the ADI BF5xx chip and SoC AC97 Audio support for BF5xx activated in kernel

 

Now I try different things in the kernel config :

 

ALSA for SoC audio support : activated in kernel

SoC Audio for the ADI BF5xx chip : activated in kernel

SoC AC97 Audio support for BF5xx : activated as module

 

---> compilation error

 

ALSA for SoC audio support : activated in kernel

SoC Audio for the ADI BF5xx chip : activated as module

SoC AC97 Audio support for BF5xx : activated as module

 

---> compilation error

 

ALSA for SoC audio support : activated as module

SoC Audio for the ADI BF5xx chip : activated as module

SoC AC97 Audio support for BF5xx : activated as module

 

---> compilation OK

 

root:~> insmod /lib/modules/2.6.22.15-ADI-2007R2-pre-svn/kernel/sound/ac97_bus.ko

root:~> insmod /lib/modules/2.6.22.15-ADI-2007R2-pre-svn/kernel/sound/soc/snd-soc-core.ko

ASoC version 0.13.1

root:~> insmod /lib/modules/2.6.22.15-ADI-2007R2-pre-svn/kernel/sound/soc/blackfin/snd-soc-bf5xx-ac97.ko

root:~> insmod /lib/modules/2.6.22.15-ADI-2007R2-pre-svn/kernel/sound/soc/blackfin/snd-soc-bf5xx.ko

root:~> insmod /lib/modules/2.6.22.15-ADI-2007R2-pre-svn/kernel/sound/soc/codecs/snd-soc-ad1980.ko

root:~> insmod /lib/modules/2.6.22.15-ADI-2007R2-pre-svn/kernel/sound/soc/blackfin/snd-ad1981.ko

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

root:~>

 

root:~> ls /dev

audio      mixer      mtdblock0  pts        ram12      ram3       ram8

console    mtd0       mtdblock1  ram0       ram13      ram4       ram9

controlC0  mtd0ro     null       ram1       ram14      ram5       zero

dsp        mtd1       pcmC0D0c   ram10      ram15      ram6

log        mtd1ro     pcmC0D0p   ram11      ram2       ram7

 

Now /dev/dsp is here !!! but there is no /dev/snd.

 

But tone doesn't work :

 

root:~> tone

ERROR: failed to open DAC device /dev/dsp

 

Do I need now to install alsa-libs ?

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2007-12-27 05:24:06     Re: Advanced usage of the AD1981B codec

Mike Frysinger (UNITED STATES)

Message: 49034    it doesnt matter what userspace libraries (like alsa-lib) you have installed ... /dev/dsp creation is completely up to the kernel and mdev

 

the important directory to look in is /sys/class/sound/ ... there needs to be a mixer and dsp subdirectory in there

QuoteReplyEditDelete

 

 

2007-12-27 05:39:08     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49035    With the audio configured as module :

 

root:~> ls -lR /sys/class/sound/

/sys/class/sound/:

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 audio -> ../../devices/platform/soc-audio/sound/card0/audio

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 card0 -> ../../devices/platform/soc-audio/sound/card0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 controlC0 -> ../../devices/platform/soc-audio/sound/card0/controlC0

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 dsp -> ../../devices/platform/soc-audio/sound/card0/dsp

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 mixer -> ../../devices/platform/soc-audio/sound/card0/mixer

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 pcmC0D0c -> ../../devices/platform/soc-audio/sound/card0/pcmC0D0c

lrwxrwxrwx    1 root     root            0 Jan  1 00:01 pcmC0D0p -> ../../devices/platform/soc-audio/sound/card0/pcmC0D0p

lrwxrwxrwx    1 root     root            0 Jan  1 00:00 timer -> ../../devices/virtual/sound/timer

 

root:~> ls -l /dev/dsp

brw-rw----    1 root     root      14,   3 Jan  1 00:01 /dev/dsp

 

 

On my laptop :

 

cat testfile > /dev/dsp

I hear sound

 

On the bf537 board :

 

root:~> cat testfile > /dev/dsp

/dev/dsp: cannot create

 

Yet, /dev/dsp is here

TranslateQuoteReplyEditDelete

 

 

2007-12-27 05:48:48     Re: Advanced usage of the AD1981B codec

Mike Frysinger (UNITED STATES)

Message: 49037    so your userspace is ok ... the device node is being created properly

 

the failure is in the kernel driver somewhere

QuoteReplyEditDelete

 

 

2007-12-27 06:04:41     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49038    The /dev/dsp is only created when I have the soc sound as module.

 

The error when opening /dev/dsp probably come from the fact that it's not an ad1980 but an ad1986.

TranslateQuoteReplyEditDelete

 

 

2007-12-27 09:15:21     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49050    Do I need to add something in the board file ?

TranslateQuoteReplyEditDelete

 

 

2007-12-29 10:36:12     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 49112    Good news !

 

I was right, it was the same error/problem than on my LQ043 topic. With the "Create deprecated sysfs files" option activated in the kernel config, I can open /dev/dsp and /dev/snd/* is well created.

 

When I launch "tone" or mp2play, I can see the sound on the LINE_OUT_R and LINE_OUT_L outputs, good !

Now the next step for me is to see how use the 6 DAC as 3 independants channels....

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2008-02-19 13:30:05     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 51292    Sorry to up this old thread..

 

The board I work on is for an electric car which will be presented to the "Geneva show" the 6-16 march 2008.

 

Thus I have some thing to finish, and the sound is the priority...

For now everything is ok with the AD1986, I use the soc driver as is (ad1980 based I believe), and it works well.

When I launch mp3play or tone or play, signals appears on the stereo outputs of the codec.

 

Yesterday I worked on the stereo amplifier part of the board (TPA3100D2 based), it works, but to do the job correctly I want to correctly setup the amplifier gain to never saturate, and I have some questions :

 

After boot, the "mixer" application tells me that "vol" is at 100, and "pcm" is at 100.

With this, if I launch tone, I have a perfect sinus on the stereo output, at maximum scale : 0V to 4.5V centered on 2.25V (4.5V peak to peak)

 

But if I play a 16 bits wav file, containing a sinus at full scale ( -32768/+32767), the signal at the codec output is completly saturated. I need to set the "pcm" to 82 to have the max amplitude value before saturate : 0.25V to 4.25V centered on 2.25V (4V peak to peak).

If set "pcm" to 83 I go in saturation.

 

What configuration I need to use to set my amplifier gain to not saturate the signal on my speaker ?

 

What I don't understand it's why a full scale 16 bits sinus goes in saturation on the codec output if the volumes are set to 100% ??

TranslateQuoteReplyEditDelete

 

 

2008-02-19 14:29:26     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 51294    Cyril:

 

Tone does not play out full scale.

 

try "tone -?" to get usage, but what I think you want is the (undocumented - will fix that) "-m" magintude option.

 

0 to 255 (255 is full scale, default is 100 (or ~ 40% of linear volume).

 

-Robin

QuoteReplyEditDelete

 

 

2008-02-19 16:45:20     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 51297    Robin, in fact it was not exactly my question. Even if tone don't generate a full scale sinus by default, I can do it with a wav file.

What I what to know is if it's a normal behavior to have the codec outputs saturated when playing a full scale sinus with "vol" and "pcm" to 100.

 

In my case, the codecs outputs are full scale and not saturated when I play my full scale wav file with "vol" to 100 and "pcm" to 82.

 

I want to undertand this because if some audio file have sounds close to the full scale and volume is 100%, the sound will be already deteriorated before the amplifier !

TranslateQuoteReplyEditDelete

 

 

2008-02-20 05:18:21     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 51332    Okay, I think I have my answer.

 

I connected a cable into the headphone of my laptop, and I tested same thing I have tested on my board, with my wav file which contain a sinus at full scale.

I used alsamixer to play with volumes.

 

When headphone volume and pcm are set to 100%, the sinus is also saturated on the output, at same level as me : 4.6V peak to peak. I need to set the pcm value to 81 to have a perfect sinus close to full scale without saturation (4.05V peak to peak). When I set pcm to 84 (I cannot find how to have a increment step of 1), the sinus begin to saturate.

 

Thus in fact I have exactly the same behavior on my board, the maximum pcm level before saturation is 82.

It is as if value above 82 amplify the original signal in fact ??

 

And when pcm is at 100, and I play with the headphone volume, the sinus stay saturated even if the output signal have low amplitude (with headphone volume to 50 for example) !!

 

Now I know it's normal I have this behavior on my board, thus I can set my amplifier gain to never saturate on the speaker with a full scale signal at input (+/-2.3V). Thus because the amplifier is powered under 12V, I need a x5.2 gain value.

 

Regards,

Cyril

TranslateQuoteReplyEditDelete

 

 

2008-02-20 11:41:06     Re: Advanced usage of the AD1981B codec

Robin Getz (UNITED STATES)

Message: 51366    Cyril:

 

It is difficult to define audio and "standard" in terms of anything.

 

<meta content="text/html; charset=utf-8" http-equiv="CONTENT-TYPE" /> <title></title> <meta content="OpenOffice.org 2.0 (Linux)" name="GENERATOR" /> <meta content="Anniep" name="AUTHOR" /> <meta content="20001031;12210000" name="CREATED" /> <meta content="ShawnPr" name="CHANGEDBY" /> <meta content="20001102;15500000" name="CHANGED" />PC2001 defines full scale output as >= 1Vrms (2.82 V peak-peak).

http://www.microsoft.com/whdc/system/platform/pcdesign/desguide/pcguides.mspx

 

Typically Windows limits the gain in the codec, and does not set the top of the slider to be the max gain.

 

I'm not sure if that answers things or not. but it is normal (but bad) for a full scale audio file to saturate the outputs at the max gain.

 

-Robin

 

QuoteReplyEditDelete

 

 

2008-02-20 11:50:34     Re: Advanced usage of the AD1981B codec

Cyril HAENEL (FRANCE)

Message: 51368    I will do the same thing in the final application : limit the gain to never saturate the codec output, even with a full scale signal in the audio file.

 

I set my amplifier gain to never saturate on the speaker, I connect 2 verygood speakers, and it's really incredible the power I have with the TPA3100D2 (class D amplifier) !!

 

With a 2000Hz tone at full scale (~18W rms), it's untenable !!

Attachments

    Outcomes