2008-02-14 07:58:41     2008R1 Build error

Document created by Aaronwu Employee on Aug 5, 2013Last modified by Aaronwu Employee on Aug 5, 2013
Version 2Show Document
  • View in full screen mode

2008-02-14 07:58:41     2008R1 Build error

Patrick Mc Donnell (IRELAND)

Message: 51047    Hi,

 

I am having problems compiling 2008R1 for the BF548.

I have installed:

blackfin-toolchain-08r1-8.i386

blackfin-toolchain-elf-gcc-4.1-08r1-8.i386

blackfin-toolchain-uclibc-full-08r1-8.i386

 

I have attached the build log.

 

Thanks,

Patrick

error_log.txt

QuoteReplyEditDelete

 

 

2008-02-14 08:19:07     Re: 2008R1 Build error

Robin Getz (UNITED STATES)

Message: 51048    Patrick:

 

What kind of host are you building on?

 

can do you a make bugreport, and attach the .tgz file too? It will include all your config files.

 

-Robin

QuoteReplyEditDelete

 

 

2008-02-14 09:09:48     Re: 2008R1 Build error

Patrick Mc Donnell (IRELAND)

Message: 51050    Robin,

 

I am using coLinux (Debian-3.0r2).

Sorry if this is a stupid question but what file would you like me to attach?

 

Patrick

QuoteReplyEditDelete

 

 

2008-02-14 09:21:17     Re: 2008R1 Build error

Robin Getz (UNITED STATES)

Message: 51053    Patrick:

 

rgetz@imhotep:~/blackfin/trunk/uClinux-dist> make bugreport

rm -f ./bugreport.tgz ./toolchain_vers ./host_vers

cc -v 2> ./host_vers

bfin-linux-uclibc-gcc -v 2> ./toolchain_vers

tar -czf bugreport.tgz .config linux-2.6.x/.config config/.config toolchain_vers host_vers

rm -f ./toolchain_vers ./host_vers

echo -e "Please attach the file 'bugreport.tgz' to a bug report at\n http://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemAdd&tracker_id=141"

Please attach the file 'bugreport.tgz' to a bug report at

http://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemAdd&tracker_id=141

 

rgetz@imhotep:~/blackfin/trunk/uClinux-dist> ls -l bugreport.tgz

-rw-r--r-- 1 rgetz users 19420 2008-02-14 09:21 bugreport.tgz

 

Does that help?

 

-Robin

QuoteReplyEditDelete

 

 

2008-02-14 10:36:35     Re: 2008R1 Build error

Patrick Mc Donnell (IRELAND)

Message: 51056    Robin,

 

Yes that helps a lot, thanks.

 

Patrick

bugreport.tgz

QuoteReplyEditDelete

 

 

2008-02-14 13:47:13     Re: 2008R1 Build error

Mike Frysinger (UNITED STATES)

Message: 51062    the sed on your system is horribly out of date ... upgrade it to the latest version:

apt-get install sed

QuoteReplyEditDelete

 

 

2008-02-15 04:37:50     Re: 2008R1 Build error

Patrick Mc Donnell (IRELAND)

Message: 51084    I upgraded sed but i'm still getting the same errors.

error_log.txt

bugreport.tgz

QuoteReplyEditDelete

 

 

2008-02-15 13:51:10     Re: 2008R1 Build error

Mike Frysinger (UNITED STATES)

Message: 51117    upgrade your findutils as well

QuoteReplyEditDelete

 

 

2008-02-20 07:27:02     Re: 2008R1 Build error

Patrick Mc Donnell (IRELAND)

Message: 51337    after updating findutils and setting blackfin build options to FDPIC, I am now getting an error with linking non-fdpic object file into fdpic executable.

bugreport.tgz

log

QuoteReplyEditDelete

 

 

2008-02-20 11:08:53     Re: 2008R1 Build error

Robin Getz (UNITED STATES)

Message: 51359    Patrick:

 

After switching file formats, you need to do a "make clean", to get rid of all the flat files.

 

-Robin

Outcomes