2008-02-17 23:45:44     Where can I download 2008R1 release package?

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-17 23:45:44     Where can I download 2008R1 release package?

Ben Lee (UNITED STATES)

Message: 51170    I only found 2007 releases from the file download page. Can some one send me the link to download all the packages? Thanks.

QuoteReplyEditDelete

 

 

2008-02-17 23:57:12     Re: Where can I download 2008R1 release package?

Mike Frysinger (UNITED STATES)

Message: 51171    2008R1 hasnt been released just yet

QuoteReplyEditDelete

 

 

2008-02-18 00:05:49     Re: Where can I download 2008R1 release package?

Ben Lee (UNITED STATES)

Message: 51173    Thanks Mike. There are 2008R1-RC3/ branches in SVN. Are they stable?  When is 2008R1 planed to be released?

QuoteReplyEditDelete

 

 

2008-02-18 00:33:47     Re: Where can I download 2008R1 release package?

Mike Frysinger (UNITED STATES)

Message: 51175    2008R1-RC3 is not a branch, it is a tag

 

the 2008R1 branch should be fine ... it'll be released when it's ready (prob in the next week or so)

QuoteReplyEditDelete

 

 

2008-02-18 00:37:20     Re: Where can I download 2008R1 release package?

Sonic Zhang (CHINA)

Message: 51177   

 

Login then http://blackfin.uclinux.org/gf/project/uclinux-dist/frs/?action=FrsReleaseView&release_id=372

 

 

QuoteReplyEditDelete

 

 

2008-02-18 03:18:20     Re: Where can I download 2008R1 release package?

murti iki (GERMANY)

Message: 51181    Hello,

I have a question regarding the toolchain, I have read the release notes and followed the link for the toolchain. but (maybe it's just me) couldn't find any explicit 2008R1 toolchain. Should I use the nightly snapshots?

 

One more question would be about the live sources. Do you think that it would be okey to run the 2008 release only by getting the new toolchain and the uclinux but NOT the u-boot. I have a custom board.

 

thanks

Attachments

    Outcomes