2008-02-13 06:06:53     Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-13 06:06:53     Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Herbert Weinfurter (AUSTRIA)

Message: 50977   

 

Kernelversion 2007R1.1 RC3

 

if I connect the board to the sport the development-boear doesn't startup!!

 

I tried to integrate the driver for 1981b once in kernel/ once as module  --> no difference

 

currently there is no auto-reset at the u-boot startup

 

the uboot basically works perfect .......... do I have to consider anything at the uboot usage?

QuoteReplyEditDelete

 

 

2008-02-14 02:07:06     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Yi Li (CHINA)

Message: 51024    Could you please post the boot log?

QuoteReplyEditDelete

 

 

2008-02-14 09:00:29     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Herbert Weinfurter (AUSTRIA)

Message: 51049   

 

until now I used the precompiled image of uboot.

 

there are no message written.

 

are there any possibilities to enable advanced logging options in UBOOT?

QuoteReplyEditDelete

 

 

2008-02-14 09:19:23     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Robin Getz (UNITED STATES)

Message: 51052    Herbert:

 

I think Yi is asking for when you say it fails - how does it fail? What prints out on the screen?

 

Thanks

-Robin

QuoteReplyEditDelete

 

 

2008-02-14 10:07:22     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Herbert Weinfurter (AUSTRIA)

Message: 51054    Following Output:

 

Excå

U-Boot 1.1.6-svn737 (ADI-2007R1) (Apr  4 2007 - 11:24:34)

 

CPU:   ADSP BF533 Rev.: 0.3

Board: ADI BF533 Stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 398 MHz, Core: 398 MHz, System: 79 MHz

SDRAM: 128 MB

FLASH:   4 MB

 

 

 

QuoteReplyEditDelete

 

 

2008-02-14 14:03:34     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Mike Frysinger (UNITED STATES)

Message: 51065    there are 2008R1 pre-release images you can test ... please grab the bf533 stamp one

QuoteReplyEditDelete

 

 

2008-02-15 03:11:15     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Herbert Weinfurter (AUSTRIA)

Message: 51081   

 

is this release compatible with 2007R1.1 kernel?

 

I'll try the

 

Nightly Snapshots     snaps     3 - Alpha     u-boot-trunk-svn.src.tar.bz2

 

OK?,  If not, give me the correct link

QuoteReplyEditDelete

 

 

2008-02-15 03:31:42     Re: Problem AD1981B on BF533-STAMP ... UBoot stops at startup

Mike Frysinger (UNITED STATES)

Message: 51083    generally speaking, u-boot and the kernel versions do not matter so long as u-boot is newer than the kernel

Attachments

    Outcomes