2008-02-06 13:42:40     Can AD7476 SPI daughter board send data over SPORT

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-06 13:42:40     Can AD7476 SPI daughter board send data over SPORT

Myrick Monroe (UNITED STATES)

Message: 50769    I just noticed from the AD7476 data sheet that the ADI 21xx DSP family serial connection for the AD7476 is the SPORT port.  Is there a reason why uClinux and the BF537 Stamp board cannot be used in this manner?  Can we use the SPORT port instead of the SPI for communication to this A/D board?

QuoteReplyEditDelete

 

 

2008-02-12 10:53:16     Re: Can AD7476 SPI daughter board send data over SPORT

Mike Frysinger (UNITED STATES)

Message: 50942    i imagine if you update the driver, you can do anything.  the driver only supports SPI communication currently.

Attachments

    Outcomes