2008-02-08 18:05:39     ad7877 touchscreen with microwindows

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-08 18:05:39     ad7877 touchscreen with microwindows

Bill Fassler (UNITED STATES)

Message: 50864    I see on www.microwindows.org that there is some mention of adding

touchscreen support as far back aas 2003. Although other than the nxcal (which I can use with the mouse at this point, but not touchscreen) I see no indication that I can configure any touchscreen support in the config file

(uClinux-dist/user/microwindows/src/config).

 

Here is something I snagged from the www.microwindows.org page:

 

* added ADS7846 touchscreen support (PSI OMAP Innovator) (Dave)

 

Has anyone managed to get the AD7877 touchscreen working with microwindows? I am using a custom BF561 board with the Sharp LQ043.

 

Bill

QuoteReplyEditDelete

 

 

2008-02-10 03:50:40     Re: ad7877 touchscreen with microwindows

Yi Li (CHINA)

Message: 50887    I saw Michael has checked in code to nanox, adding support of ad7877.

Attachments

    Outcomes