2008-02-06 19:56:44     Are the Nightly Snapshots current?

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-06 19:56:44     Are the Nightly Snapshots current?

Frank Van Hooft (CANADA)

Message: 50788    Just wondering if the nightly snapshots, particularly the SVN Trunk tarball, are actually current?  I pulled down one of the image logfiles & noticed it contained a build date of October 2007.

 

I want to do a full SVN update; doing it this way:

 

svn checkout svn://sources.blackfin.uclinux.org/uclinux-dist/trunk uclinux-dist

 

is a 1.6 GB download. But the bzipped source tarball is only a bit over 200 MB. So if the tarballs are current, that would save this site (and me) a great deal of bandwidth.

 

Thanks.

QuoteReplyEditDelete

 

 

2008-02-07 00:15:52     Re: Are the Nightly Snapshots current?

Mike Frysinger (UNITED STATES)

Message: 50790    they are not updated at the moment as the build machine is offline due to hardware failure ... hopefully it'll be back up later this month

QuoteReplyEditDelete

 

 

2008-02-07 00:57:59     Re: Are the Nightly Snapshots current?

Frank Van Hooft (CANADA)

Message: 50795    Thanks!

Attachments

    Outcomes