2008-02-06 06:34:41     What file load to board?

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-06 06:34:41     What file load to board?

Anton Romanov (RUSSIAN FEDERATION)

Message: 50753    Hi

 

make what write on page:

<a target="_blank" href="http://docs.blackfin.uclinux.org/doku.php?id=basic_compilation">http://docs.blackfin.uclinux<wbr></wbr>.org/doku.php?id=basic_compila<wbr></wbr>tion

 

and take some files on images direction:

linux.ext2

rootfs.ext2

rootfs.jffs2

rootfs.yaffs

rootfs.yaffs2

ulmage.ext2

vmimage

vmlinux

 

so, what file i need to load to the board?

 

p.s.on page:

<a target="_blank" href="../../gf/project/uclinux-dist/frs/">http://blackfin.uclinux.org/gf<wbr></wbr>/project/uclinux-dist/frs/

files:

uImage-bf537-stamp-2007R1.1-RC3

linux-bf537-stamp-2007R1.1-RC

Can i load one of this files or for what these files are necessary?

 

Thanks for help.

QuoteReplyEditDelete

 

 

2008-02-06 08:45:59     Re: What file load to board?

Yi Li (CHINA)

Message: 50757   

 

> uImage-bf537-stamp-2007R1.1-RC3 ,linux-bf537-stamp-2007R1.1-RC

 

uImage is the compressed version of linux.

 

vmImage/vmlinux is the kernel image, if combined with rootfs.(ext2,jffs2,yaff2), that would be linux.(ext2..).

Attachments

    Outcomes