2008-02-05 08:21:37     errors at compilation uCLinux

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-02-05 08:21:37     errors at compilation uCLinux

Anton Romanov (RUSSIAN FEDERATION)

Message: 50693    Hi

 

Do what write on page:

<a target="_blank" href="http://docs.blackfin.uclinux.org/doku.php?id=basic_compilation">http://docs.blackfin.uclinux<wbr></wbr>.org/doku.php?id=basic_compila<wbr></wbr>tion

 

 

Use : ADZS-BF537-EZKit Lite

     blackfin-toolchain-07r1.1-3

<wbr></wbr>.i386.rpm

     uClinux-dist-2007R1.1-RC3.tar<wbr></wbr>.bz2

 

When i have some errors:

..

bfin-uclinux-gcc -I../libc/include -O2 -pipe -fno-builtin -Wall   -DEMBED -D__uClinux__ -isystem /root/uclinux-dist/uClinux-dist.R1.1-RC3/staging/usr/include -g -DFLOATS=1 -DL_printf ../libc/stdio2/printf.c -c -o printf.o

In file included from ../libc/stdio2/printf.c:27:

../libc/include/stdarg.h:3:28: error: machine/stdarg.h: Рет такого файла или каталога

In file included from ../libc/stdio2/printf.c:34:

../libc/include/stdio.h:125: error: expected declaration specifiers or

...

 

error say what i not have file machine/stdarg.h .

it is true. this file must have some function used on prinf.c

 

Why this file can not be available?

 

Thanks for the help.

QuoteReplyEditDelete

 

 

2008-02-05 10:40:08     Re: errors at compilation uCLinux

Mike Frysinger (UNITED STATES)

Message: 50700    you selected the "uC-libc" library in the toplevel menuconfiguration option ... do not do that.  just leave the default of "none".

Attachments

    Outcomes