2008-01-31 20:13:05     compile libbfgdots err with uClinux-dist-2008R1-RC1

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-01-31 20:13:05     compile libbfgdots err with uClinux-dist-2008R1-RC1

w w (CHINA)

Message: 50524   

 

when i compile libbfgdots under uClinux-dist-2008R1-RC1 , the err is:

 

make[1]: Entering directory `/uClinux-2008/lib'

[ -z "" ] || make -j1  || exit $?

[ -z "" ] || (cd /uClinux-2008/staging; chmod 755 ./usr/lib/lib*.so*; chmod 644 ./usr/lib/lib*.la ./usr/lib/lib*.a; sed -i "/^libdir=/s:=.*:='/uClinux-2008/staging/usr/lib':" ./usr/lib/*.la; sed -i "/^prefix=/s:=.*:='/uClinux-2008/staging/usr':" ./usr/lib/pkgconfig/*.pc ./usr/bin/*-config; true)

[ -z "" ] || make -j1  || exit $?

[ -z "" ] || (cd /uClinux-2008/staging; chmod 755 ./usr/lib/lib*.so*; chmod 644 ./usr/lib/lib*.la ./usr/lib/lib*.a; sed -i "/^libdir=/s:=.*:='/uClinux-2008/staging/usr/lib':" ./usr/lib/*.la; sed -i "/^prefix=/s:=.*:='/uClinux-2008/staging/usr':" ./usr/lib/pkgconfig/*.pc ./usr/bin/*-config; true)

[ -z "libg zlib libjpeg libbfgdots" ] || make -j1 libbfgdots libg libjpeg zlib || exit $?

make[2]: Entering directory `/uClinux-2008/lib'

make -C libbfgdots

make[3]: Entering directory `/uClinux-2008/lib/libbfgdots'

make -C g729

make[4]: Entering directory `/uClinux-2008/lib/libbfgdots/g729'

make -C test

make[5]: Entering directory `/uClinux-2008/lib/libbfgdots/g729/test'

bfin-uclinux-gcc -I ../include/ -Wall -DG729_MULTI_INST -o g729ab_test.o -c g729ab_test.c

g729ab_test.c:33:19: error:dlfcn.h:No such file or directory

make[5]: *** [g729ab_test.o] error 1

make[5]: Leaving directory `/uClinux-2008/lib/libbfgdots/g729/test'

make[4]: *** [all] error 2

make[4]: Leaving directory `/uClinux-2008/lib/libbfgdots/g729'

make[3]: *** [g729_all] error 2

make[3]: Leaving directory `/uClinux-2008/lib/libbfgdots'

make[2]: *** [libbfgdots] error 2

make[2]: Leaving directory `/uClinux-2008/lib'

make[1]: *** [all] error 2

make[1]: Leaving directory `/uClinux-2008/lib'

make: *** [subdirs] error 1

 

i can find the dlfcn.h in   /opt/uClinux/bfin-linux-uclibc/bfin-linux-uclibc/runtime/usr/include/dlfcn.h, but I can not compile it, can you help me ?

 

i use the toolchain 08r1, thank you!!!

QuoteReplyEditDelete

 

 

2008-01-31 20:37:25     Re: compile libbfgdots err with uClinux-dist-2008R1-RC1

Mike Frysinger (UNITED STATES)

Message: 50528    should be fixed in svn now ... please do not use the 2008R1 release until it has been released

Attachments

    Outcomes