2008-01-25 05:12:19     increase stack with bfin-linux-uclibc

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-01-25 05:12:19     increase stack with bfin-linux-uclibc

Piggebu Piggebu (ANDORRA)

Message: 50129    Hi all

 

I am facing the following problem:

I have precompiled libraries, compiled with the bfin-linux-uclibc toolchain.

Now I am trying to compile my own programme which uses these libraries. A sample worked fine while compiling with the bfin-linux-uclibc, however, the full programme needs more memory on the stack.

 

If the precompiled libraries were compiled with the bfin-uclinux toolchain this would work with:

bfin-uclinux-gcc -Wl,-elf2flt="-s 8192" application.c

(from http://docs.blackfin.uclinux.org/doku.php?id=debuging_applications)

 

how do I increase now the stack with the bfin-linux-uclibc toolchain?

 

Regards

Piggebu

 

 

PS: namely I would need the libusb library in the bfin-linux-uclibc format... however to compile it myself standalone without the  dist-config tools would be a challenge for me :-/

QuoteReplyEditDelete

 

 

2008-01-25 06:39:39     Re: increase stack with bfin-linux-uclibc

Mike Frysinger (UNITED STATES)

Message: 50140    the document you quoted already says how to change the stack size for FDPIC ELF ... just scroll down to the next section right after the FLAT one you've read

QuoteReplyEditDelete

 

 

2008-01-25 11:09:05     Re: increase stack with bfin-linux-uclibc

Piggebu Piggebu (ANDORRA)

Message: 50153    Hi Mike,

 

sorry about my lazy investigations... your hint solved the problem, the programme works fine.

 

Thanks

Piggebu

Attachments

    Outcomes