2008-01-22 12:25:15     Image does not start!

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-01-22 12:25:15     Image does not start!

Hans Huber (GERMANY)

Message: 49960    Hi,

 

i just created a new image and flashed it into my BF537. I did not changed much things in the menuconfig. Just disactivated some app programms which i don't need. When i flash the board an reset it it does not start it. It halts at "Starting kernel at = 1000" (see below)

 

## Booting image at 20100000 ...

   Image Name:   uClinux Kernel Image

   Created:      2008-01-22  17:10:03 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2454924 Bytes =  2.3 MB

   Load Address: 00001000

   Entry Point:  00001000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 1000

 

Does anybody have an idea?

QuoteReplyEditDelete

 

 

2008-01-22 17:29:11     Re: Image does not start!

Mike Frysinger (UNITED STATES)

Message: 49970    please see this page:

http://docs.blackfin.uclinux.org/doku.php?id=post_mortem

Attachments

    Outcomes