2008-01-18 08:03:34     STAMP reseting alone

Document created by Aaronwu Employee on Aug 5, 2013
Version 1Show Document
  • View in full screen mode

2008-01-18 08:03:34     STAMP reseting alone

Joao Paulo Bodanese (BRAZIL)

Message: 49801    Hi,

 

When i try to load an image, my stamp reset and show the error:

 

bf537> tftp 0x1000000 image

Link is down, please check your network connection

Using BF537 ETHERNET device

TFTP from server 192.168.61.55; our IP address is 192.168.0.15

Filename 'image'.

Load address: 0x1000000

Loading: code=[0x24], stack frame=0x3f9b9bc, bad PC=0x3fc0158

 

 

Unhandled IRQ or exceptions!

Please reset the board

icache_enable

U-Boot 1.1.6-svn737 (ADI-2007R1) (Apr  4 2007 - 11:42:51)

 

CPU:   ADSP BF537 Rev.: 0.2

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 100 MHz

SDRAM: 64 MB

FLASH:   4 MB

In:    serial

Out:   serial

Err:   serial

Net:    BF537 ETHERNET

I2C:   ready

Hit any key to stop autoboot:  0

## Error: "tftpboot" not defined

bf537>            

 

 

Any idea?               

QuoteReplyEditDelete

 

 

2008-01-18 14:13:25     Re: STAMP reseting alone

Mike Frysinger (UNITED STATES)

Message: 49810    your network is not connected and u-boot currently crashes if you attempt to use it when it is not connected

Attachments

    Outcomes