2008-01-14 06:42:27     Trouble with bridging

Document created by Aaronwu Employee on Aug 4, 2013
Version 1Show Document
  • View in full screen mode

2008-01-14 06:42:27     Trouble with bridging

Alex Noskov (RUSSIAN FEDERATION)

Message: 49550    Hi. I have two ethernet interfaces(eth0, eth1), and two hdlc interfaces(hdlc0, hdlc1). I want to do bridge: eth0<->hdlc0 eth1<->hdlc1 I must create bridge without using of bridge-utils. When I try to use iproute2 I can't create rule(I don't know why): #ip rule show #ip rule add from all table 200 #ip rule show # How to do the bridge?

QuoteReplyEditDelete

 

 

2008-01-14 22:20:16     Re: Trouble with bridging

Yi Li (CHINA)

Message: 49573    Maybe you can post the mailing list mentioned here for help: http://www.linux-foundation.org/en/Net:Bridge.

Attachments

    Outcomes