2008-01-10 16:21:00     SPI CS is not a "1"

Document created by Aaronwu Employee on Aug 4, 2013
Version 1Show Document
  • View in full screen mode

2008-01-10 16:21:00     SPI CS is not a "1"

Alex Stewart (UNITED STATES)

Message: 49458    Hi,

So Ive been trying to get the SPI worked out for a few weeks now. And I think I've finally made it through understanding the framework. I have one problem however. With an o-scope connected up, I can see my CLK and MOSI send my data correctly and my CS line does "frame" my data, but it idles at 1.1V  not ~2.5V like CLK and MOSI......

 

I thought this may be because of a missing pullup, but even with a 1K pull up on the CS line I cant get it to idle at >~1V.... My device is active low, but it still thinks it is selected even when CS  is "idle"....

 

Any ideas?

 

Im using the SPI framework, Slave Select #5 on a BF537-STAMP board....

 

And its not the ADC im connected to, because the CS acts the same with or without the ADC connected....

 

Thanks for the Help!!!!

QuoteReplyEditDelete

 

 

2008-01-14 21:43:02     Re: SPI CS is not a "1"

Bryan Wu (CHINA)

Message: 49570    Hi Alex,

 

Did you modified any source code to do this test?

CS can be controlled by software driver or user space application.

Maybe a bug I fixed several days ago can be a reference for you.

https://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemEdit&tracker_item_id=3821

 

-Bryan Wu

Attachments

    Outcomes