2008-01-07 18:27:55     mplayer complilation error at rev

Document created by Aaronwu Employee on Aug 4, 2013
Version 1Show Document
  • View in full screen mode

2008-01-07 18:27:55     mplayer complilation error at rev

Ozgur Bulkan (TURKEY)

Message: 49339   

I have recently downloaded uclinux distribution and compiled tree successfully for BF561 silicon num 3.

 

When mplayer is selected in configuration, its link fails as attached command line output file.

 

Release number is 5956 and "gcc version" is 4.1.2 (ADI svn)

 

What could be the reason? Best regards, Ozgur

 

 

 

 

command_out

QuoteReplyEditDelete

 

 

2008-01-07 19:24:02     Re: mplayer complilation error at rev

Mike Frysinger (UNITED STATES)

Message: 49340    mplayer will not currently work for FLAT ... use FDPIC ELF

QuoteReplyEditDelete

 

 

2008-01-07 21:27:39     Re: mplayer complilation error at rev

Yi Li (CHINA)

Message: 49342    Can we set default build format as FDPIC, or force to select FDPIC when selecting mplayer, linphone, vlc, etc, which require FDPIC format?

QuoteReplyEditDelete

 

 

2008-01-07 21:56:35     Re: mplayer complilation error at rev

Mike Frysinger (UNITED STATES)

Message: 49343    that depends on whether we want to prevent people from being able to build as FLAT at all ... it wouldnt be hard to make it work under FLAT, it'll just be a performance trade off

Attachments

    Outcomes