What are the number formats for SigmaDSP?

Document created by BrettG on Aug 1, 2013Last modified by BrettG on Aug 1, 2013
Version 3Show Document
  • View in full screen mode

Question:

In the SigmaStudio help file, some of the algorithms have input and outputs specified as integer or decimal. Also, in the SigmaDSP datasheets, there are references to 28.0 and 5.23. Also, in SigmaStudio, sometimes cells will have other formats like 5.19. What does this mean?

 

Answer:

SigmaDSP systems use a standardized fixed-point number format. Fixed-point numbers are formatted A.B, where A is the number of bits to the left of the decimal point (the integer part) and B is the number of bits to the right of the decimal point (the fractional part).

 

Inputs to the SigmaDSP cores are 24 bits. In the core, the DSP adds 4 additional zeros for additional headroom. The result is a 28 bit number representation.

 

So, in the case of most SigmaDSPs, audio representation is represented with A = 5 and B = 23. In other words, the number format is 5.23. Control signals and index table values generally require integer representation, and are therefore represented with A = 28 and B = 0. In other words, the format is 28.0.

 

28.0 (Integer) Format

 

Signals that are in integer format follow standard binary rules for representation.
0 = 0, 1 = 1, 10 = 2, 11 = 3, 100 = 4, et cetera.
Including zero padding (and 4 extra bits to make a 4-byte, 32-bit word for the control port), positive integers in the DSP are represented as follows:

 

0000 0000 0000 0000 0000 0000 0000 0000 = 0
0000 0000 0000 0000 0000 0000 0000 0001 = 1
0000 0000 0000 0000 0000 0000 0000 0010 = 2
0000 0000 0000 0000 0000 0000 0000 0011 = 3
0000 0000 0000 0000 0000 0000 0000 0100 = 4
...
0000 0000 1000 0000 0000 0000 0000 0000 = 8388608 (0 dB full scale represented in 28.0 format)
...
0000 0111 1111 1111 1111 1111 1111 1111 = 134217727 (2^27 - 1)

 

Negative numbers are represented in two's complement. For more information on two's complement, please read the very comprehensive article on Wikipedia here: http://en.wikipedia.org/wiki/Two%27s_complement

 

The corresponding 28-bit two's complement integers (with 4 bits added on top for the control port) are represented as follows:

 

1111 1000 0000 0000 0000 0000 0000 0000 = -134217728 (2^27)
...
1111 1111 1111 1111 1111 1111 1111 1100 = -4
1111 1111 1111 1111 1111 1111 1111 1101 = -3
1111 1111 1111 1111 1111 1111 1111 1110 = -2
1111 1111 1111 1111 1111 1111 1111 1111 = -1

 

In general, negative integers are not used in SigmaStudio or SigmaDSP algorithms.

 

When outputting to the serial ports or DACs, signals will saturate at 0 dBFS. This means any signal exceeding 8388608 in 28.0 format will be limited to full-scale on the outputs.

 

5.23 (Decimal) Format

 

Audio, unlike control signals, is not represented as an integer, but rather as a decimal value. A full-scale audio signal has an amplitude of 1. If -3 dB of gain is applied, it should have an amplitude of approximately 0.707. If -6 dB of gain is applied, the signal has an amplitude of 0.5. So, it is easy to see that audio signals need to be represented as decimal numbers.

 

A full scale 24-bit input signal would have a positive peak of 1000 0000 0000 0000 0000 0000 in unsigned, 24-bit representation. If we add 4 bits of headroom, the 28-bit representation becomes 0000 1000 0000 0000 0000 0000 0000. There is also an additional nibble (4 bits) added on top to make the total word length 4 bytes, which makes the 32-bit representation 0000 0000 1000 0000 0000 0000 0000 0000. If two's-complement representation is used, then the negative peak of a full-scale signal becomes 1111 1111 1000 0000 0000 0000 0000 0000.

 

The top 4 bits, used to make a whole number of bytes for the control port, are actually ignored inside the DSP. So, the top 4 bits are effectively "don't care."

 

Moving the leading '1' to the left or right will double or halve the value, respectively.

 

0000 0000 0000 0000 0000 0000 0000 0000 =  0.0
0000 0000 0010 0000 0000 0000 0000 0000 =  0.25
0000 0000 0100 0000 0000 0000 0000 0000 =  0.5
0000 0000 1000 0000 0000 0000 0000 0000 =  1.0 (0 dB full scale)
0000 0001 0000 0000 0000 0000 0000 0000 =  2.0
0000 0010 0000 0000 0000 0000 0000 0000 =  4.0
0000 0111 1111 1111 1111 1111 1111 1111 =  (16.0 - 1 LSB)

 

For negative numbers, signed two's-complement is used.

 

1111 1000 0000 0000 0000 0000 0000 0000 =  -16.0
1111 1110 0000 0000 0000 0000 0000 0000 =  -4.0

1111 1111 0000 0000 0000 0000 0000 0000 =  -1.0
1111 1111 1000 0000 0000 0000 0000 0000 =  -1.0
1111 1111 1100 0000 0000 0000 0000 0000 =  -0.5
1111 1111 1110 0000 0000 0000 0000 0000 =  -0.25
1111 1111 1111 1111 1111 1111 1111 1111 =  (1 LSB below 0.0)

 

When outputting to the serial ports or DACs, signals will saturate at 0 dBFS. This means any signal with a peak exceeding 1.0 in 5.23 format will be limited to full-scale on the outputs.

 

5.27 (Decimal) Format (ADAU1772)

A full scale 24-bit input signal would have a positive peak of 1000 0000 0000 0000 0000 0000 in unsigned, 24-bit representation. If we add 4 bits of headroom, the 28-bit representation becomes 0000 1000 0000 0000 0000 0000 0000. The ADAU1772 has an additional four bits for extended precision so this then becomes 0000 1000 0000 0000 0000 0000 0000 0000. If two's-complement representation is used, then the negative peak of a full-scale signal becomes 1111 1000 0000 0000 0000 0000 0000 0000.

 

Moving the leading '1' to the left or right will double or halve the value, respectively.

 

0000 0000 0000 0000 0000 0000 0000 0000 =  0.0
0000 0010 0000 0000 0000 0000 0000 0000 =  0.25
0000 0100 0000 0000 0000 0000 0000 0000 =  0.5
0000 1000 0000 0000 0000 0000 0000 0000 =  1.0 (0 dB full scale)
0001 0000 0000 0000 0000 0000 0000 0000 =  2.0
0010 0000 0000 0000 0000 0000 0000 0000 =  4.0
0111 1111 1111 1111 1111 1111 1111 1111 =  (16.0 - 1 LSB)

 

For negative numbers, signed two's-complement is used.

 

1000 0000 0000 0000 0000 0000 0000 0000 =  -16.0
1110 0000 0000 0000 0000 0000 0000 0000 =  -4.0
1111 0000 0000 0000 0000 0000 0000 0000 =  -1.0
1111 1000 0000 0000 0000 0000 0000 0000 =  -1.0
1111 1100 0000 0000 0000 0000 0000 0000 =  -0.5
1111 1110 0000 0000 0000 0000 0000 0000 =  -0.25
1111 1111 1111 1111 1111 1111 1111 1111 =  (1 LSB below 0.0)

 

5.19 (Hardware readback) Format

 

Some cells in SigmaStudio may use slightly different number formats. For example, since the hardware-based DSP readback registers in the ADAU1701 only have 24 bits, the lower 4 bits from the 5.23 signal are truncated and the number is represented in 5.19 format.

 

So, a full-scale signal that was represented in 5.23 format as
0000 1000 0000 0000 0000 0000 0000
would have its lower 4 bits truncated for 5.19 representation:
0000 1000 0000 0000 0000 0000

 

The result is that very small amplitude signals will be truncated and therefore cannot be read back from the DSP on the older generation of SigmaDSP cores.

 

Newer cores, such as the ADAU1761 and ADAU144x, have full 5.23 readback capabilities implemented in software.

 

Question:

From the datasheet:

The parameter RAM is 32 bits wide and occupies Address 0 to Address 1023. Each parameter is padded with four 0s before the MSB to extend the 28-bit word to a full 4-byte width.

 

If writing these values from a microcontroller, do we have to ensure that these padding bits are always 0, or is their value ignored?

 

Answer:

The value of the top 4 bits will be ignored. Only the 28 LSBs matter. So, you can write 0x0FFFFFFF or 0xFFFFFFFF to the control port, and the DSP will regard them as the same number.

 

This FAQ was generated from the following discussion: What are the number formats for SigmaDSP?

Attachments

    Outcomes