Notes about the crystal neeeded for the ADV7180 or ADV7182

Document created by Rob.Analog on Jul 9, 2013
Version 1Show Document
  • View in full screen mode

A 28.63636 MHz fundamental frequency crystal is needed to clock the ADV7180 or ADV7182.

 

This crystal needs a tolerance of +/- 50 ppm over the temperature range of operation.

 

For analog devices evaluation boards a Golledge MA01377 crystal is used. ( see attached datasheet).

 

 

Notes on using an oscillator to clock the ADV7180 instead of a crystal:

http://ez.analog.com/thread/19637

 

Notes on using an oscillator to clock the ADV7182 instead of a crysta:

http://ez.analog.com/thread/19638

Attachments

Outcomes