FAQ; Incline Output Response and Format

Document created by NevadaMark Employee on Feb 4, 2013Last modified by NevadaMark Employee on Feb 4, 2013
Version 2Show Document
  • View in full screen mode

Q:

I am evaluating the ADIS16210 on the EVAL-ADIS evaluation system and was wondering if you could explain the output data format from the IMU Evaluation software?

----------------------------------------------------------------------------------------------------------------------------------------

A:

The incline data uses a 16-bit, twos complement format.  The register responses depend on the MSC_CTRL register.  See pages 9, 10, 12 and 13 in the ADIS16210 (rev A) datasheet for a more complete explanation of the sensor response, as this response will offer an example to address this question.

ADIS16210 Datasheet: http://www.analog.com/static/imported-files/data_sheets/ADIS16210.pdf

 

Step #1

Use the ADIS16210/EVAL-ADIS Wiki Guide to install the ADIS16210/PCBZ onto the EVAL-ADIS and install the IMU Evaluation software package onto your test PC.

 

Step #2

Once that is working, go into the Register Access menu to set DIO_CTRL = 0x000, AVG_CNT = 0x0003 and MSC_CTRL = 0x0002.

FAQ-16210-01-RegSet.png

 

Step #3

Then, go into the Data Capture menu, select XINCL_OUT, set the total number of samples and set the datalog filename/path.

 

FAQ-16210-01-DataCapt.png

 

Step #4

Hit Start and then slowly tilt the sensor around the X-axis. this picture shows a tilt in the negative x-direction.

210-NegX.JPG

 

Here is an example of the sensor response. The file attachment illustrates the process of converting the binary number (twos complement format) into a decimal representation.

FAQ-16210-01-Response.png

Hope that helps. As always, we appreciate your comments and look forward to hearing from you!

Best,

NevadaMark

Outcomes