ADV7623 Design Support Files

Document created by joe.triggs Employee on Nov 22, 2012Last modified by joe.triggs Employee on Jul 21, 2016
Version 10Show Document
  • View in full screen mode

The ADV7623 is a 4-input, 1-output HDMI transceiver which supports Xpressview fast switching and a character- and icon-based OSD.

 

This page contains the key support documents and configuration settings that a user of the ADV7623 requires; these are attached and linked below. The ADV7623 is also supported with a comprehensive software driver which features a reference OSD design. For more information on this software driver, please contact your local ADI sales office.

 

Product support for the supported modes is provided through the Engineer Zone forum.

ItemDescription
ADV7623 Product PageLink to Product Page
ADV7623 DatasheetLink to ADV7623 Datasheet
Additional Support Documents
ADV7623 Hardware Manual

Hardware Manual containing descriptions of the salient controls and their functions

(file attached below in ADV7623_Documentation.zip)

ADV7623 Software Manual

Software Manual containing descriptions of the register maps

(file attached below in ADV7623_Documentation.zip)

ADV7623 Recommended Settings

Recommended Settings guide containing the recommended initial settings and required algorithms

(file attached below in ADV7623_Documentation.zip)

ADV7623 Evaluation Board User GuideEvaluation Board User Guide (file attached below in ADV7623_Documentation.zip)
Script file
ADV7623-Ver1-12Cust.txt.Configuration scripts for ADV7623 (file attached below)
Reference Schematics & Layout
ADV7623 Evaluation Board Schematic

Evaluation board reference schematic

(file attached below in see ADV7623_Eval_Board_RevD.zip)

ADV7623 Evaluation Board Layout

Evaluation board reference layout

(file attached below in see ADV7623_Eval_Board_RevD.zip)

OSD

ADV7623_OSD_Software_Programmer's

_Guide_PrD.pdf

Programmer's Guide which provides information on functionality and features supported by the ADV7623 OSD block, the OSD engine API library and how to program the OSD generated code to the platform. (file attached below)

ADV7623_Character-Based_OSD_Tool

_User_Guide_Rev._0.10.pdf

User guide which describes how to create an OSD using the Character-based OSD tool and provides a detailed description of how the user can employ the tool to develop a customised OSD for the ADV7623. (file attached below)

AVES Board File
AVES3_EVAL-ADV7623EBZ_20160105.zipAVES3 folder for the EVAL-ADV7623EBZ evaluation board
Software
Software package for ADV7623 evaluation board

Download HPM software package for ADV7623 evaluation board here.

 

For documentation on software, it will be posted shortly.

 

The Character-based OSD tool is available from Analog Devices' Software Request website - www.analog.com/srf. Please select "Other" for the hardware platform and put "ADV7623 OSD Tool" in the comments.

Outcomes