MLVDS FAQ: Why should I use a 100Mbps device instead of a 200Mbps device?

Document created by ColmR Employee on Nov 12, 2012
Version 1Show Document
  • View in full screen mode

Q: Why should I use a 100Mbps M-LVDS transceiver instead of a 200Mbps M-LVDS transceiver?



In transmission line theory, it is best practice to use a part with a rise and fall time as close to the data rate required to minimize reflections.  ADI provides two datarates to facilitate this: 100Mbps for datarates up to 100Mbps and 200Mbps for applications that need datarates between 100Mbps and 200Mbps.


For more MLVDS information, please visit the topic page: