cm3wsd Version 2

File uploaded by ABuda Employee on Oct 23, 2012Last modified by ABuda Employee on Jan 24, 2018
Version 2Show Document
  • View in full screen mode

We've worked on a new version of the cm3wsd downloader which adds a few improvements.

Some of the improvements include:

All the settings are now available in the main window;

A cancel button was added;

Automatic scanning of COM ports so only available ports will be displayed;

An experimental autoflash feature where once all the settings are set and the start button is pressed, multiple eval boards can be flashed without interacting with the program.

 

This is a BETA version so bugs might still be present.

 

Feedback will be greatly appreciated

Attachments

Outcomes