Empty Cells

Document created by BrettG on Oct 15, 2012
Version 1Show Document
  • View in full screen mode


As I drag items from the Toolbox into the schematic tab, sometimes the items come in blank (i.e. instead of the expected control such as a general second order filter I get and empty hierarchical type block). Why is this happening?





This behavior happens when multiple possible algorithms are tied to a single graphical control. In this case, you need to right-click the cell and select “Add Algorithm”, and then choose the desired algorithm from the list. After that, the cell GUI should appear.


Here’s an example with a filter:


When I select the one I want…

…the GUI populates.