Using ADAU1761 for microphone beamforming

Document created by BrettG on Oct 9, 2012
Version 1Show Document
  • View in full screen mode

We used an ADAU1761 to create a simple microphone beamforming application, with two omnidirectional ADMP504 MEMS microphones mounted in an endfire configuration.

 

Using the attached Excel sheet to perform the calculations, we calculated that a total of 6 samples of delay are required to generate a delay appropriate for a microphone spacing of 42 mm at a sample rate of 48 kHz.

 

Distance between microphones (mm)42
Speed of sound (mm per sample @ 48 kHz)7
Samples to cover microphone distance @ 48 kHz6

 

The following project was created to realize the signal flow.

 

2012.10.09 11.23.53.jpg

Reference materials:

Microphone Beamforming Application Note

ADMP504 MEMS Microphone Datasheet

ADAU1761 Datasheet

Outcomes