FAQ: What are the system requirements for CCES?

Document created by DavidS on Sep 19, 2012Last modified by DavidS on Aug 28, 2013
Version 4Show Document
  • View in full screen mode

Q: What operating systems can I install CCES on and what are the minimum requirements?

 

-----------

 

A: The system requirements are:

  • Minimum of 2 GHz single core processor, 3.3 GHz dual core is recommended.
  • Minimum of 1 GB memory (RAM), 4 GB is recommended.
  • Minimum of 2 GB hard disk (HDD) space is required.

    

Also, a faster disk drive will decrease the build time, especially for a large amount of source files.

 

CCES is supported on the following Windows operating systems:

  • Windows XP SP3 (32-bit version only)
  • Windows Vista Business/Enterprise/Ultimate SP2 (32-bit version only)
  • Windows 7 Professional/Enterprise/Ultimate (32-bit and 64-bit versions)

 

From CCES 1.0.2 onwards the following operating system is also supported:

  • Windows 8 Profesional/Enterprise (32-bit and 64-bit versions). 

 

 

 

Note; CCES does not install into a User Access Control (UAC) directory. The default installation path is:

C:\Analog Devices\CrossCore Embedded Studio, however, Windows Vista, Windows 7 and Windows 8 users may experience User Access Control (UAC) related errors if the software is installed into a protected location such as “Program Files” or “Program Files (x86)”.If you wish to change the default install path we recommend using a non-UAC-protected location.

Attachments

    Outcomes